TIMER_InitCC_TypeDef Struct ReferenceEMLIB > TIMER
TIMER compare/capture initialization structure.
       Definition at line
       
        357
       
       of file
       
        em_timer.h
       
       .
      
      
       #include <
       
     
        em_timer.h
       
       >
      
Field Documentation
| TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa | 
Counter match output action.
        Definition at line
        
         377
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa | 
Counter overflow output action.
        Definition at line
        
         374
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| bool TIMER_InitCC_TypeDef::coist | 
Compare output initial state. Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.
        Definition at line
        
         395
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa | 
Counter underflow output action.
        Definition at line
        
         371
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge | 
Input capture edge select.
        Definition at line
        
         362
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl | 
Input capture event control.
        Definition at line
        
         359
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| bool TIMER_InitCC_TypeDef::filter | 
| TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode | 
Compare/capture channel mode.
        Definition at line
        
         380
        
        of file
        
         em_timer.h
        
        .
       
Referenced by BOARD_init() , TIMER_InitCC() , USBTIMER_Init() , and USTIMER_Init() .
| bool TIMER_InitCC_TypeDef::outInvert | 
Invert output from compare/capture channel.
        Definition at line
        
         398
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| bool TIMER_InitCC_TypeDef::prsInput | 
Select TIMERnCCx (false) or PRS input (true).
        Definition at line
        
         386
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_PrsOutput_t TIMER_InitCC_TypeDef::prsOutput | 
PRS output configuration. PRS output from a timer can either be a pulse output or a level output that follows the CC out value.
        Definition at line
        
         404
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
| TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel | 
        Peripheral reflex system trigger selection. Only applicable if
        
         prsInput
        
        is enabled.
       
        Definition at line
        
         368
        
        of file
        
         em_timer.h
        
        .
       
Referenced by TIMER_InitCC() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_timer.h