SMUEMLIB
Detailed Description
Security Management Unit (SMU) Peripheral API.
SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.
Peripheral-level protection is provided via the peripheral protection unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.
Data Structures | |
struct | SMU_Init_TypeDef |
struct | SMU_PrivilegedAccess_TypeDef |
Macros | |
#define | SMU_INIT_DEFAULT |
Enumerations | |
enum | SMU_Peripheral_TypeDef { smuPeripheralACMP0 = _SMU_PPUPATD0_ACMP0_SHIFT, smuPeripheralACMP1 = _SMU_PPUPATD0_ACMP1_SHIFT, smuPeripheralADC0 = _SMU_PPUPATD0_ADC0_SHIFT, smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT, smuPeripheralCRYOTIMER = _SMU_PPUPATD0_CRYOTIMER_SHIFT, smuPeripheralCRYPTO = _SMU_PPUPATD0_CRYPTO0_SHIFT, smuPeripheralVDAC0 = _SMU_PPUPATD0_VDAC0_SHIFT, smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT, smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT, smuPeripheralFPUEH = _SMU_PPUPATD0_FPUEH_SHIFT, smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT, smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT, smuPeripheralI2C0 = _SMU_PPUPATD0_I2C0_SHIFT, smuPeripheralIDAC0 = _SMU_PPUPATD0_IDAC0_SHIFT, smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT, smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT, smuPeripheralLESENSE = _SMU_PPUPATD0_LESENSE_SHIFT, smuPeripheralLETIMER0 = _SMU_PPUPATD0_LETIMER0_SHIFT, smuPeripheralLEUART = _SMU_PPUPATD0_LEUART0_SHIFT, smuPeripheralPCNT0 = _SMU_PPUPATD0_PCNT0_SHIFT, smuPeripheralRMU = _SMU_PPUPATD0_RMU_SHIFT, smuPeripheralRTCC = _SMU_PPUPATD0_RTCC_SHIFT, smuPeripheralSMU = _SMU_PPUPATD0_SMU_SHIFT, smuPeripheralTIMER0 = 32 + _SMU_PPUPATD1_TIMER0_SHIFT, smuPeripheralTIMER1 = 32 + _SMU_PPUPATD1_TIMER1_SHIFT, smuPeripheralTRNG0 = 32 + _SMU_PPUPATD1_TRNG0_SHIFT, smuPeripheralUSART0 = 32 + _SMU_PPUPATD1_USART0_SHIFT, smuPeripheralUSART1 = 32 + _SMU_PPUPATD1_USART1_SHIFT, smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT, smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT, smuPeripheralWTIMER0 = 32 + _SMU_PPUPATD1_WTIMER0_SHIFT, smuPeripheralEnd } |
Functions | |
__STATIC_INLINE void | SMU_EnablePPU (bool enable) |
Enable or disable PPU of SMU. | |
__STATIC_INLINE SMU_Peripheral_TypeDef | SMU_GetFaultingPeripheral (void) |
Get ID of the peripheral that caused an access fault. | |
__STATIC_INLINE void | SMU_Init (const SMU_Init_TypeDef *init) |
Initialize PPU of SMU. | |
__STATIC_INLINE void | SMU_IntClear (uint32_t flags) |
Clear one or more pending SMU interrupts. | |
__STATIC_INLINE void | SMU_IntDisable (uint32_t flags) |
Disable one or more SMU interrupts. | |
__STATIC_INLINE void | SMU_IntEnable (uint32_t flags) |
Enable one or more SMU interrupts. | |
__STATIC_INLINE uint32_t | SMU_IntGet (void) |
Get pending SMU interrupts. | |
__STATIC_INLINE uint32_t | SMU_IntGetEnabled (void) |
Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
__STATIC_INLINE void | SMU_IntSet (uint32_t flags) |
Set one or more pending SMU interrupts from SW. | |
__STATIC_INLINE void | SMU_SetPrivilegedAccess (SMU_Peripheral_TypeDef peripheral, bool privileged) |
Change access settings for a peripheral. | |
Macro Definition Documentation
#define SMU_INIT_DEFAULT |
Default SMU initialization structure settings.
Definition at line 911
of file em_smu.h
.
Enumeration Type Documentation
SMU peripheral identifiers.
Definition at line 78
of file em_smu.h
.
Function Documentation
__STATIC_INLINE void SMU_EnablePPU | ( | bool | enable | ) |
Enable or disable PPU of SMU.
- Parameters
-
[in] enable
Set to true to enable PPU; set to false otherwise.
Definition at line 927
of file em_smu.h
.
References BUS_RegBitWrite().
Referenced by SMU_Init().
__STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral | ( | void |
| ) |
Get ID of the peripheral that caused an access fault.
- Note
- The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.
- Returns
- ID of the peripheral that caused an access fault.
Definition at line 989
of file em_smu.h
.
__STATIC_INLINE void SMU_Init | ( | const SMU_Init_TypeDef * | init | ) |
Initialize PPU of SMU.
- Parameters
-
[in] init
Pointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.
Definition at line 944
of file em_smu.h
.
References SMU_Init_TypeDef::enable, SMU_Init_TypeDef::reg, and SMU_EnablePPU().
__STATIC_INLINE void SMU_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending SMU interrupts.
- Parameters
-
[in] flags
Bitwise logic OR of SMU interrupt sources to clear.
Definition at line 1001
of file em_smu.h
.
__STATIC_INLINE void SMU_IntDisable | ( | uint32_t | flags | ) |
Disable one or more SMU interrupts.
- Parameters
-
[in] flags
SMU interrupt sources to disable.
Definition at line 1017
of file em_smu.h
.
__STATIC_INLINE void SMU_IntEnable | ( | uint32_t | flags | ) |
Enable one or more SMU interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
SMU interrupt sources to enable.
Definition at line 1038
of file em_smu.h
.
__STATIC_INLINE uint32_t SMU_IntGet | ( | void |
| ) |
Get pending SMU interrupts.
- Returns
- SMU interrupt sources pending.
Definition at line 1054
of file em_smu.h
.
__STATIC_INLINE uint32_t SMU_IntGetEnabled | ( | void |
| ) |
Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by this function.
- Returns
- Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in SMU_IEN register and
- the OR combination of valid interrupt flags in SMU_IF register.
Definition at line 1074
of file em_smu.h
.
__STATIC_INLINE void SMU_IntSet | ( | uint32_t | flags | ) |
Set one or more pending SMU interrupts from SW.
- Parameters
-
[in] flags
SMU interrupt sources to set to pending.
Definition at line 1093
of file em_smu.h
.
__STATIC_INLINE void SMU_SetPrivilegedAccess | ( | SMU_Peripheral_TypeDef | peripheral, |
bool | privileged |
||
) |
Change access settings for a peripheral.
Set to limit access of a peripheral from privileged mode.
- Parameters
-
[in] peripheral
ID of the peripheral to change access settings for. [in] privileged
Set to true if the peripheral should only be accessed from privileged mode; set to false otherwise.
Definition at line 966
of file em_smu.h
.
References BUS_RegBitWrite().