VddCheckKit Drivers

Detailed Description

VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API.

Functions

void VDDCHECK_Disable (void)
 VCMP deinitialization routine.
 
void VDDCHECK_Init (void)
 VCMP initialization routine.
 
bool VDDCHECK_LowVoltage (float vdd)
 Check if voltage is higher than indicated.
 

Function Documentation

bool VDDCHECK_LowVoltage ( float  vdd)

Check if voltage is higher than indicated.

Parameters
vddThe voltage level to compare against.
Returns
Returns true if voltage is lower, false otherwise

Definition at line 68 of file vddcheck.c.