ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC

Scan sequence initialization structure.

Definition at line 864 of file em_adc.h.

#include <em_adc.h>

Data Fields

ADC_AcqTime_TypeDef acqTime
 
bool diff
 
bool fifoOverwrite
 
bool leftAdjust
 
bool prsEnable
 
ADC_PRSSEL_TypeDef prsSel
 
ADC_Ref_TypeDef reference
 
bool rep
 
ADC_Res_TypeDef resolution
 
bool scanDmaEm2Wu
 
ADC_InitScanInput_TypeDef scanInputConfig
 

Field Documentation

ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime

Acquisition time (in ADC clock cycles).

Definition at line 872 of file em_adc.h.

Referenced by ADC_InitScan().

bool ADC_InitScan_TypeDef::diff

Select if single-ended or differential input.

Definition at line 902 of file em_adc.h.

Referenced by ADC_InitScan(), ADC_ScanDifferentialInputAdd(), and ADC_ScanSingleEndedInputAdd().

bool ADC_InitScan_TypeDef::fifoOverwrite

When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.

Definition at line 921 of file em_adc.h.

Referenced by ADC_InitScan().

bool ADC_InitScan_TypeDef::leftAdjust

Select if left adjustment should be done.

Definition at line 908 of file em_adc.h.

Referenced by ADC_InitScan().

bool ADC_InitScan_TypeDef::prsEnable

Peripheral reflex system trigger enable.

Definition at line 905 of file em_adc.h.

Referenced by ADC_InitScan(), and MIC_init().

ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 869 of file em_adc.h.

Referenced by ADC_InitScan(), and MIC_init().

ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference

Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.

Definition at line 878 of file em_adc.h.

Referenced by ADC_InitScan(), and MIC_init().

bool ADC_InitScan_TypeDef::rep

Select if continuous conversion until explicit stop.

Definition at line 911 of file em_adc.h.

Referenced by ADC_InitScan().

ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution

Sample resolution.

Definition at line 881 of file em_adc.h.

Referenced by ADC_InitScan().

bool ADC_InitScan_TypeDef::scanDmaEm2Wu

When true, DMA is available in EM2 for scan conversion

Definition at line 915 of file em_adc.h.

Referenced by ADC_InitScan(), and MIC_init().

ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig

Scan input configuration. Use ADC_ScanInputClear(), ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this structure.

Definition at line 898 of file em_adc.h.

Referenced by ADC_InitScan(), ADC_ScanDifferentialInputAdd(), ADC_ScanInputClear(), and ADC_ScanSingleEndedInputAdd().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/em_adc.h