UARTDRV_InitUart_t Struct ReferenceEMDRV > UARTDRV

A UART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required for driver instance initialization. This structure is passed to UARTDRV_Init() when initializing a UARTDRV instance.

Definition at line 179 of file uartdrv.h.

#include <uartdrv.h>

Data Fields

uint32_t baudRate
 UART baud rate.
 
uint8_t ctsPin
 A CTS pin number.
 
GPIO_Port_TypeDef ctsPort
 A CTS pin port number.
 
UARTDRV_FlowControlType_t fcType
 Flow control mode.
 
bool mvdis
 Majority Vote Disable for 16x, 8x and 6x oversampling modes.
 
USART_OVS_TypeDef oversampling
 Oversampling mode.
 
USART_Parity_TypeDef parity
 Parity configuration.
 
USART_TypeDef * port
 The peripheral used for UART.
 
uint8_t portLocationCts
 A location number for the UART CTS pin.
 
uint8_t portLocationRts
 A location number for the UART RTS pin.
 
uint8_t portLocationRx
 A location number for UART Rx pin.
 
uint8_t portLocationTx
 A location number for UART Tx pin.
 
uint8_t rtsPin
 An RTS pin number.
 
GPIO_Port_TypeDef rtsPort
 An RTS pin port number.
 
UARTDRV_Buffer_FifoQueue_trxQueue
 A receive operation queue.
 
USART_Stopbits_TypeDef stopBits
 A number of stop bits.
 
UARTDRV_Buffer_FifoQueue_ttxQueue
 T transmit operation queue.
 

The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/uartdrv/inc/uartdrv.h