ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC
Single conversion initialization structure.
Definition at line
964
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
ADC_SingleInput_TypeDef | input |
bool | leftAdjust |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line
972
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .
bool ADC_InitSingle_TypeDef::diff |
Select if single-ended or differential input.
Definition at line
1003
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input |
Sample input selection, use single-ended or differential input according to setting of
diff
.
Definition at line
988
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .
bool ADC_InitSingle_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line
1009
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
bool ADC_InitSingle_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line
1006
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsEnable
is enabled.
Definition at line
969
of file
em_adc.h
.
Referenced by ADC_InitSingle() , and adcInit() .
ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference |
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
Definition at line
978
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .
bool ADC_InitSingle_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line
1012
of file
em_adc.h
.
Referenced by ADC_InitSingle() .
ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution |
Sample resolution.
Definition at line
981
of file
em_adc.h
.
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_adc.h