DMA_Init_TypeDef Struct ReferenceEMLIB > DMA

DMA initialization structure.

Definition at line 303 of file em_dma.h .

#include < em_dma.h >

Data Fields

DMA_DESCRIPTOR_TypeDef * controlBlock
uint8_t hprot

Field Documentation

DMA_DESCRIPTOR_TypeDef* DMA_Init_TypeDef::controlBlock

Pointer to the control block in memory holding descriptors (channel control data structures). This memory must be properly aligned at a 256 bytes, i.e., the 8 least significant bits must be zero.

Refer to the reference manual, DMA chapter for more details.

It is possible to provide a smaller memory block, only covering those channels actually used, if not all available channels are used. For instance, if only using 4 channels (0-3), both primary and alternate structures, then only 16*2*4 = 128 bytes must be provided. However, this implementation has no check if later exceeding such a limit by configuring for instance channel 4, in which case memory overwrite of some other data will occur.

Definition at line 329 of file em_dma.h .

Referenced by DMA_Init() .

uint8_t DMA_Init_TypeDef::hprot

HPROT signal state when accessing the primary/alternate descriptors. Normally set to 0 if protection is not an issue. The following bits are available:

  • bit 0 - HPROT[1] control for descriptor accesses (i.e., when the DMA controller accesses the channel control block itself), privileged/non-privileged access.

Definition at line 312 of file em_dma.h .

Referenced by DMA_Init() .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_dma.h