EMU_DCDCInit_TypeDef Struct ReferenceEMLIB > EMU
DCDC initialization structure.
Definition at line
761
of file
em_emu.h
.
#include <
em_emu.h
>
Field Documentation
EMU_DcdcAnaPeripheralPower_TypeDef EMU_DCDCInit_TypeDef::anaPeripheralPower |
Select analog peripheral power in DCDC-to-DVDD mode.
Definition at line
778
of file
em_emu.h
.
EMU_DcdcLnCompCtrl_TypeDef EMU_DCDCInit_TypeDef::dcdcLnCompCtrl |
DCDC Low-noise mode compensator control.
Definition at line
785
of file
em_emu.h
.
EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::dcdcMode |
DCDC regulator operating mode in EM0/1.
Definition at line
764
of file
em_emu.h
.
Referenced by BSP_initDcdc() .
uint16_t EMU_DCDCInit_TypeDef::em01LoadCurrent_mA |
Estimated average load current in EM0/1. (mA). This estimate is also used for EM1 optimization; if EM1 current is expected to be higher than EM0, then this parameter should hold the higher EM1 current.
Definition at line
766
of file
em_emu.h
.
uint16_t EMU_DCDCInit_TypeDef::em234LoadCurrent_uA |
Estimated average load current in EM2 (uA). This estimate is also used for EM3 and 4 optimization; if EM3 or 4 current is expected to be higher than EM2, then this parameter should hold the higher EM3 or 4 current.
Definition at line
770
of file
em_emu.h
.
uint16_t EMU_DCDCInit_TypeDef::maxCurrent_mA |
Maximum average DCDC output current (mA). This can be set to the maximum for the power source, for example the maximum for a battery.
Definition at line
774
of file
em_emu.h
.
uint16_t EMU_DCDCInit_TypeDef::mVout |
Target output voltage (mV).
Definition at line
765
of file
em_emu.h
.
EMU_PowerConfig_TypeDef EMU_DCDCInit_TypeDef::powerConfig |
Device external power configuration. emuPowerConfig_DcdcToDvdd is currently the only supported mode.
Definition at line
762
of file
em_emu.h
.
EMU_DcdcLnReverseCurrentControl_TypeDef EMU_DCDCInit_TypeDef::reverseCurrentControl |
Low-noise reverse current control. NOTE: this parameter uses special encoding: >= 0 is forced CCM mode where the parameter is used as the reverse current threshold in mA. -1 is encoded as emuDcdcLnHighEfficiencyMode (EFM32 only).
Definition at line
780
of file
em_emu.h
.
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_emu.h