MSC_ExecConfig_TypeDef Struct ReferenceEMLIB > MSC

Code execution configuration.

Definition at line 164 of file em_msc.h .

#include < em_msc.h >

Data Fields

bool aiDis
bool iccDis
bool ifcDis
bool prefetchEn
bool scbtEn
bool useHprot

Field Documentation

bool MSC_ExecConfig_TypeDef::aiDis

Disable automatic cache invalidation on write or erase.

Definition at line 168 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .

bool MSC_ExecConfig_TypeDef::iccDis

Disable automatic caching of fetches in interrupt context.

Definition at line 169 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .

bool MSC_ExecConfig_TypeDef::ifcDis

Disable instruction cache.

Definition at line 167 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .

bool MSC_ExecConfig_TypeDef::prefetchEn

Enable MSC prefetching.

Definition at line 166 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .

bool MSC_ExecConfig_TypeDef::scbtEn

Enable Suppressed Conditional Branch Target Prefetch.

Definition at line 165 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .

bool MSC_ExecConfig_TypeDef::useHprot

Use ahb_hprot to determine if the instruction is cacheable or not.

Definition at line 170 of file em_msc.h .

Referenced by MSC_ExecConfigSet() .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_msc.h