EZRADIODRV_PacketRxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Receive_Plugin

EzRadio receive plug-in instance initialization and handler structure.

Definition at line 50 of file ezradio_receive_plugin.h.

#include <ezradio_receive_plugin.h>

Data Fields

uint8_t channel
 Reception channel.
 
uint8_t * pktBuf
 Pointer to the receive buffer.
 
EZRADIODRV_Callback_t userCallback
 User callback.
 

The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emdrv/ezradiodrv/plugins/inc/ezradio_receive_plugin.h