ezradio_comm.c File Reference

This file contains the EZRadio communication layer.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
  3. This notice may not be removed or altered from any source distribution.

Definition in file ezradio_comm.c.

#include <stdint.h>
#include <stdarg.h>
#include "em_gpio.h"
#include "gpiointerrupt.h"
#include "ustimer.h"
#include "ezradiodrv_config.h"
#include "ezradio_hal.h"
#include "ezradio_comm.h"

Functions

void ezradio_comm_ClearCTS ()
 
uint8_t ezradio_comm_GetResp (uint8_t byteCount, uint8_t *pData)
 
uint8_t ezradio_comm_PollCTS (void)
 
void ezradio_comm_ReadData (uint8_t cmd, uint8_t pollCts, uint8_t byteCount, uint8_t *pData)
 
void ezradio_comm_SendCmd (uint8_t byteCount, uint8_t *pData)
 
uint8_t ezradio_comm_SendCmdGetResp (uint8_t cmdByteCount, uint8_t *pCmdData, uint8_t respByteCount, uint8_t *pRespData)
 
void ezradio_comm_WriteData (uint8_t cmd, uint8_t pollCts, uint8_t byteCount, uint8_t *pData)
 

Variables

uint8_t ezradio_comm_CtsWentHigh = 0