VDAC
Detailed Description
Digital to Analog Voltage Converter (VDAC) Peripheral API.
This module contains functions to control the VDAC peripheral of Silicon Labs' 32-bit MCUs and SoCs. VDAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. VDAC is designed for low energy consumption, but can also provide very good performance.
The following steps are necessary for basic operation:
Clock enable:
Initialize the VDAC with default settings and modify selected fields:
Perform a conversion:
- Note
- The output stage of a VDAC channel consists of an on-chip operational amplifier (OPAMP) in the OPAMP module. This OPAMP is highly configurable; and to exploit the VDAC functionality fully, configure the OPAMP using the OPAMP API. Using the OPAMP API also loads OPAMP calibration values. The default (reset) settings of OPAMP is sufficient for many applications.
Data Structures |
|
| struct | VDAC_Init_TypeDef |
| struct | VDAC_InitChannel_TypeDef |
Macros |
|
| #define | VDAC_INIT_DEFAULT |
| #define | VDAC_INITCHANNEL_DEFAULT |
Enumerations |
|
| enum |
VDAC_PrsSel_TypeDef
{
vdacPrsSelCh0 = _VDAC_CH0CTRL_PRSSEL_PRSCH0, vdacPrsSelCh1 = _VDAC_CH0CTRL_PRSSEL_PRSCH1, vdacPrsSelCh2 = _VDAC_CH0CTRL_PRSSEL_PRSCH2, vdacPrsSelCh3 = _VDAC_CH0CTRL_PRSSEL_PRSCH3, vdacPrsSelCh4 = _VDAC_CH0CTRL_PRSSEL_PRSCH4, vdacPrsSelCh5 = _VDAC_CH0CTRL_PRSSEL_PRSCH5, vdacPrsSelCh6 = _VDAC_CH0CTRL_PRSSEL_PRSCH6, vdacPrsSelCh7 = _VDAC_CH0CTRL_PRSSEL_PRSCH7 } |
| enum |
VDAC_Ref_TypeDef
{
vdacRef1V25Ln = _VDAC_CTRL_REFSEL_1V25LN, vdacRef2V5Ln = _VDAC_CTRL_REFSEL_2V5LN, vdacRef1V25 = _VDAC_CTRL_REFSEL_1V25, vdacRef2V5 = _VDAC_CTRL_REFSEL_2V5, vdacRefAvdd = _VDAC_CTRL_REFSEL_VDD, vdacRefExtPin = _VDAC_CTRL_REFSEL_EXT } |
| enum |
VDAC_Refresh_TypeDef
{
vdacRefresh8 = _VDAC_CTRL_REFRESHPERIOD_8CYCLES, vdacRefresh16 = _VDAC_CTRL_REFRESHPERIOD_16CYCLES, vdacRefresh32 = _VDAC_CTRL_REFRESHPERIOD_32CYCLES, vdacRefresh64 = _VDAC_CTRL_REFRESHPERIOD_64CYCLES } |
| enum |
VDAC_TrigMode_TypeDef
{
vdacTrigModeSw = _VDAC_CH0CTRL_TRIGMODE_SW, vdacTrigModePrs = _VDAC_CH0CTRL_TRIGMODE_PRS, vdacTrigModeRefresh = _VDAC_CH0CTRL_TRIGMODE_REFRESH, vdacTrigModeSwPrs = _VDAC_CH0CTRL_TRIGMODE_SWPRS, vdacTrigModeSwRefresh = _VDAC_CH0CTRL_TRIGMODE_SWREFRESH, vdacTrigModeLesense = _VDAC_CH0CTRL_TRIGMODE_LESENSE } |
Functions |
|
| __STATIC_INLINE void | VDAC_Channel0OutputSet (VDAC_TypeDef *vdac, uint32_t value) |
|
Set the output signal of VDAC channel 0 to a given value.
|
|
| __STATIC_INLINE void | VDAC_Channel1OutputSet (VDAC_TypeDef *vdac, uint32_t value) |
|
Set the output signal of VDAC channel 1 to a given value.
|
|
| void | VDAC_ChannelOutputSet (VDAC_TypeDef *vdac, unsigned int channel, uint32_t value) |
|
Set the output signal of a VDAC channel to a given value.
|
|
| void | VDAC_Enable (VDAC_TypeDef *vdac, unsigned int ch, bool enable) |
|
Enable/disable the VDAC channel.
|
|
| void | VDAC_Init (VDAC_TypeDef *vdac, const VDAC_Init_TypeDef *init) |
|
Initialize VDAC.
|
|
| void | VDAC_InitChannel (VDAC_TypeDef *vdac, const VDAC_InitChannel_TypeDef *init, unsigned int ch) |
|
Initialize a VDAC channel.
|
|
| __STATIC_INLINE void | VDAC_IntClear (VDAC_TypeDef *vdac, uint32_t flags) |
|
Clear one or more pending VDAC interrupts.
|
|
| __STATIC_INLINE void | VDAC_IntDisable (VDAC_TypeDef *vdac, uint32_t flags) |
|
Disable one or more VDAC interrupts.
|
|
| __STATIC_INLINE void | VDAC_IntEnable (VDAC_TypeDef *vdac, uint32_t flags) |
|
Enable one or more VDAC interrupts.
|
|
| __STATIC_INLINE uint32_t | VDAC_IntGet (VDAC_TypeDef *vdac) |
|
Get pending VDAC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | VDAC_IntGetEnabled (VDAC_TypeDef *vdac) |
|
Get enabled and pending VDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | VDAC_IntSet (VDAC_TypeDef *vdac, uint32_t flags) |
|
Set one or more pending VDAC interrupts from SW.
|
|
| uint32_t | VDAC_PrescaleCalc (uint32_t vdacFreq, bool syncMode, uint32_t hfperFreq) |
|
Calculate the prescaler value used to determine VDAC clock.
|
|
| void | VDAC_Reset (VDAC_TypeDef *vdac) |
|
Reset VDAC to same state that it was in after a hardwares reset.
|
|
Macro Definition Documentation
| #define VDAC_INIT_DEFAULT |
Default configuration for VDAC initialization structure.
Definition at line
192
of file
em_vdac.h
.
| #define VDAC_INITCHANNEL_DEFAULT |
Default configuration for VDAC channel initialization structure.
Definition at line
228
of file
em_vdac.h
.
Enumeration Type Documentation
| enum VDAC_PrsSel_TypeDef |
Peripheral Reflex System signal used to trigger VDAC channel conversion.
Definition at line
120
of file
em_vdac.h
.
| enum VDAC_Ref_TypeDef |
Reference voltage for VDAC.
Definition at line
110
of file
em_vdac.h
.
| enum VDAC_Refresh_TypeDef |
Channel conversion trigger mode.
Definition at line
144
of file
em_vdac.h
.
Function Documentation
| __STATIC_INLINE void VDAC_Channel0OutputSet | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
value
|
||
| ) |
Set the output signal of VDAC channel 0 to a given value.
This function sets the output signal of VDAC channel 0 by writing
value
to the CH0DATA register.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] valueValue to write to channel 0 output register CH0DATA.
Definition at line
264
of file
em_vdac.h
.
Referenced by VDAC_ChannelOutputSet() .
| __STATIC_INLINE void VDAC_Channel1OutputSet | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
value
|
||
| ) |
Set the output signal of VDAC channel 1 to a given value.
This function sets the output signal of VDAC channel 1 by writing
value
to the CH1DATA register.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] valueValue to write to channel 1 output register CH1DATA.
Definition at line
285
of file
em_vdac.h
.
Referenced by VDAC_ChannelOutputSet() .
| void VDAC_ChannelOutputSet | ( | VDAC_TypeDef * |
vdac,
|
| unsigned int |
channel,
|
||
| uint32_t |
value
|
||
| ) |
Set the output signal of a VDAC channel to a given value.
This function sets the output signal of a VDAC channel by writing
value
to the corresponding CHnDATA register.
- Parameters
-
[in] vdacA pointer to the VDAC peripheral register block. [in] channelA channel number to set the output of. [in] valueA value to write to the channel output register CHnDATA.
Definition at line
288
of file
em_vdac.c
.
References VDAC_Channel0OutputSet() , and VDAC_Channel1OutputSet() .
| void VDAC_Enable | ( | VDAC_TypeDef * |
vdac,
|
| unsigned int |
ch,
|
||
| bool |
enable
|
||
| ) |
Enable/disable the VDAC channel.
- Parameters
-
[in] vdacA pointer to the VDAC peripheral register block. [in] chA channel to enable/disable. [in] enableTrue to enable VDAC channel, false to disable.
Definition at line
79
of file
em_vdac.c
.
| void VDAC_Init | ( | VDAC_TypeDef * |
vdac,
|
| const VDAC_Init_TypeDef * |
init
|
||
| ) |
Initialize VDAC.
Initializes the common parts for both channels. This function will also load calibration values from the Device Information (DI) page into the VDAC calibration register. To complete a VDAC setup, channel control configuration must also be done. See VDAC_InitChannel() .
- Note
- This function will disable both channels prior to configuration.
- Parameters
-
[in] vdacA pointer to the VDAC peripheral register block. [in] initA pointer to the VDAC initialization structure.
Definition at line
121
of file
em_vdac.c
.
References VDAC_Init_TypeDef::asyncClockMode , VDAC_Init_TypeDef::ch0ResetPre , VDAC_Init_TypeDef::diff , VDAC_Init_TypeDef::mainCalibration , VDAC_Init_TypeDef::outEnablePRS , VDAC_Init_TypeDef::prescaler , VDAC_Init_TypeDef::reference , VDAC_Init_TypeDef::refresh , VDAC_Init_TypeDef::sineEnable , vdacRef1V25 , vdacRef1V25Ln , vdacRef2V5 , vdacRef2V5Ln , vdacRefAvdd , vdacRefExtPin , and VDAC_Init_TypeDef::warmupKeepOn .
| void VDAC_InitChannel | ( | VDAC_TypeDef * |
vdac,
|
| const VDAC_InitChannel_TypeDef * |
init,
|
||
| unsigned int |
ch
|
||
| ) |
Initialize a VDAC channel.
- Parameters
-
[in] vdacA pointer to the VDAC peripheral register block. [in] initA pointer to the VDAC channel initialization structure. [in] chA channel number to initialize.
Definition at line
224
of file
em_vdac.c
.
References VDAC_InitChannel_TypeDef::enable , VDAC_InitChannel_TypeDef::prsAsync , VDAC_InitChannel_TypeDef::prsSel , VDAC_InitChannel_TypeDef::sampleOffMode , and VDAC_InitChannel_TypeDef::trigMode .
| __STATIC_INLINE void VDAC_IntClear | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending VDAC interrupts.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] flagsPending VDAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
Definition at line
303
of file
em_vdac.h
.
| __STATIC_INLINE void VDAC_IntDisable | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
flags
|
||
| ) |
Disable one or more VDAC interrupts.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] flagsVDAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
Definition at line
319
of file
em_vdac.h
.
| __STATIC_INLINE void VDAC_IntEnable | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
flags
|
||
| ) |
Enable one or more VDAC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using VDAC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] flagsVDAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
Definition at line
340
of file
em_vdac.h
.
| __STATIC_INLINE uint32_t VDAC_IntGet | ( | VDAC_TypeDef * |
vdac
|
) |
Get pending VDAC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block.
- Returns
- VDAC interrupt sources pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
Definition at line
359
of file
em_vdac.h
.
| __STATIC_INLINE uint32_t VDAC_IntGetEnabled | ( | VDAC_TypeDef * |
vdac
|
) |
Get enabled and pending VDAC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled VDAC interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in VDACx_IEN_nnn register (VDACx_IEN_nnn) and
- the OR combination of valid interrupt flags of the VDAC module (VDACx_IF_nnn).
Definition at line
383
of file
em_vdac.h
.
| __STATIC_INLINE void VDAC_IntSet | ( | VDAC_TypeDef * |
vdac,
|
| uint32_t |
flags
|
||
| ) |
Set one or more pending VDAC interrupts from SW.
- Parameters
-
[in] vdacPointer to VDAC peripheral register block. [in] flagsVDAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the VDAC module (VDAC_IF_nnn).
Definition at line
402
of file
em_vdac.h
.
| uint32_t VDAC_PrescaleCalc | ( | uint32_t |
vdacFreq,
|
| bool |
syncMode,
|
||
| uint32_t |
hfperFreq
|
||
| ) |
Calculate the prescaler value used to determine VDAC clock.
The VDAC clock is given by the input clock divided by the prescaler+1.
VDAC_CLK = IN_CLK / (prescale + 1)
The maximum VDAC clock is 1 MHz. The input clock is HFPERCLK/HFPERCCLK when VDAC synchronous mode is selected, or an internal oscillator of 10 MHz +/- 20% when asynchronous mode is selected.
- Note
- If the requested VDAC frequency is low and the maximum prescaler value can't adjust the actual VDAC frequency lower than requested, the maximum prescaler value is returned resulting in a higher VDAC frequency than requested.
- Parameters
-
[in] vdacFreqVDAC frequency target. The frequency will automatically be adjusted to be below maximum allowed VDAC clock. [in] syncModeSet to true if you intend to use VDAC in synchronous mode. [in] hfperFreqFrequency in Hz of HFPERCLK/HFPERCCLK oscillator. Set to 0 to use the currently defined HFPERCLK/HFPERCCLK clock setting. This parameter is only used when syncMode is set to true.
- Returns
-
A prescaler value to use for VDAC to achieve a clock value less than or equal to
vdacFreq.
Definition at line
337
of file
em_vdac.c
.
References CMU_ClockFreqGet() , and cmuClock_VDAC0 .
| void VDAC_Reset | ( | VDAC_TypeDef * |
vdac
|
) |
Reset VDAC to same state that it was in after a hardwares reset.
- Parameters
-
[in] vdacA pointer to the VDAC peripheral register block.
Definition at line
381
of file
em_vdac.c
.