Direct_Transmit_Plugin
Detailed Description
Direct transmit plugin, see Plugin System Layer for detailed documentation.
.
Data Structures | |
struct | EZRADIODRV_DirectTxHandle |
EzRadio direct tx plug-in instance initialization and handler structure. | |
Macros | |
#define | EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct tx plug-in. | |
Typedefs | |
typedef struct EZRADIODRV_DirectTxHandle | EZRADIODRV_DirectTxHandle_t |
EzRadio direct tx plug-in instance initialization and handler structure. | |
Functions | |
Ecode_t | ezradioStartDirectTransmit (EZRADIODRV_Handle_t radioHandle) |
Starts direct transmission with the radio configurations from the radioHandle parameter. | |
Ecode_t | ezradioStopDirectTransmit (void) |
Stops direct transmission. | |
Macro Definition Documentation
#define EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct tx plug-in.
Definition at line 71
of file ezradio_direct_transmit_plugin.h
.
Function Documentation
Ecode_t ezradioStartDirectTransmit | ( | EZRADIODRV_Handle_t | radioHandle | ) |
Starts direct transmission with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line 54
of file ezradio_direct_transmit_plugin.c
.
References EZRADIODRV_DirectTxHandle::channel, EZRADIODRV_HandleData::directTx, ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED, ezradio_get_int_status(), ezradio_request_device_state(), and ezradio_start_tx().
Ecode_t ezradioStopDirectTransmit | ( | void |
| ) |
Stops direct transmission.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line 85
of file ezradio_direct_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK, and ezradio_change_state().