NORFLASH_Info_TypeDef Struct Reference

NORFLASH device information struct.

Definition at line 63 of file norflash.h.

#include <norflash.h>

Data Fields

uint32_t baseAddress
 
uint32_t bootSectorCount
 
uint32_t bootSectorSize
 
uint8_t deviceArc
 
uint32_t deviceId
 
uint32_t deviceSize
 
uint16_t manufacturerId
 
uint32_t sectorCount
 
uint32_t sectorSize
 
uint16_t writeBufferSize
 

Field Documentation

uint32_t NORFLASH_Info_TypeDef::baseAddress

The device base address in cpu memory map.

Definition at line 64 of file norflash.h.

Referenced by NORFLASH_AddressValid(), and NORFLASH_EraseDevice().

uint32_t NORFLASH_Info_TypeDef::bootSectorCount

Number of boot sectors in the device.

Definition at line 70 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::bootSectorSize

Boot sector size in bytes.

Definition at line 71 of file norflash.h.

Referenced by NORFLASH_EraseSector(), and NORFLASH_Program().

uint8_t NORFLASH_Info_TypeDef::deviceArc

The device sector architecture.

Definition at line 73 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::deviceId

The device ID.

Definition at line 65 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::deviceSize

Total device size in bytes.

Definition at line 66 of file norflash.h.

Referenced by NORFLASH_AddressValid().

uint16_t NORFLASH_Info_TypeDef::manufacturerId

The device manufacturer ID.

Definition at line 67 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::sectorCount

Number of sectors in the device.

Definition at line 68 of file norflash.h.

uint32_t NORFLASH_Info_TypeDef::sectorSize

Sector size in bytes.

Definition at line 69 of file norflash.h.

Referenced by NORFLASH_EraseSector(), and NORFLASH_Program().

uint16_t NORFLASH_Info_TypeDef::writeBufferSize

Write buffer size of the device.

Definition at line 72 of file norflash.h.

Referenced by NORFLASH_Program().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/norflash.h