Modules

Here is a list of all modules:
BSP Board Support Package
API for DKs
API for STKs and WSTKs
Common BSP for all kits
Device Initialization Device Initialization using HAL configuration
Thunderboard Sense BSP BSP for Thunderboard Sense and Thunderboard Sense 2
BAP - Barometric Pressure Sensor Driver for the Bosch Sensortec BMP280 pressure sensor
BOARD Module for Thunderboard Sense Board hardware control, configuraton and miscellaneous functions
Power and Interrupt Controller Definitions Thunderboard Sense 1 Power and Interrupt Controller register and bitfield definitions
BOARD Module for Thunderboard Sense 2 Board hardware control, configuraton and miscellaneous functions
CCS811 - Indoor Air Quality Sensor Driver for the Cambridge CMOS Sensors CCS811 gas and indoor air quality sensor
HALL - Hall Effect Sensor Driver for Hall effect sensor
Si7210 - Hall Effect Sensor Driver for the Silicon Labs Si7210 Hall effect sensor
ICM20648 - 6-axis Motion Sensor Driver Driver for the Invensense ICM20648 6-axis motion sensor
IMU - Inertial Measurement Unit Inertial Measurement Unit driver
MIC - Microphone Driver (ADC) Driver for the Knowles SPV1840LR5H-B MEMS Microphone
MIC - Microphone Driver (I2S) Driver for the Invensense ICS-43434 MEMS Microphone
SI1133 - Ambient Light and UV Index Sensor Driver for the Silicon Labs Si1133 Ambient Light and UV sensor
SI7021 - Relative Humidity and Temperature Sensor Driver for the Silicon Labs Si7021 I2C Humidity and Temperature Sensor
Utility Functions Utility functions
Devices Silicon Laboratories CMSIS-CORE device system headers
EFR32
EMDRV Gecko Platform driver library
DMADRV DMADRV Direct Memory Access Driver
EZRADIODRV EZR32 EzRadio Peripheral Interface Driver
API_Layer EzRadio API Layer


         
COMM_Layer EzRadio Communication Layer


         
HAL_Layer EzRadio HAL Layer


         
Plugin_System EzRadio Plugin System Layer, see Plugin System Layer for detailed documentation.


         
Auto_ACK_Plugin Auto acknowledge plugin, see Plugin System Layer for detailed documentation.


         
CRC_Error_Plugin CRC error plugin, see Plugin System Layer for detailed documentation.


         
Direct_Receive_Plugin Direct receive plugin, see Plugin System Layer for detailed documentation.


         
Direct_Transmit_Plugin Direct transmit plugin, see Plugin System Layer for detailed documentation.


         
PN9_Plugin Pseudo random transmit plugin, see Plugin System Layer for detailed documentation.


         
Plugin_Manager Plugin manager, see Plugin System Layer for detailed documentation.


         
Receive_Plugin Receive plugin, see Plugin System Layer for detailed documentation.


         
Transmit_Plugin Transmit plugin, see Plugin System Layer for detailed documentation.


         
Unmod_Carrier_Plugin Unmodulated Carrier plugin, see Plugin System Layer for detailed documentation.


         
GPIOINT GPIOINT General Purpose Input/Output Interrupt dispatcher
NVM NVM Non-volatile Memory Wear-Leveling Driver
NVM3 NVM3 Non-Volatile Memory Management driver
NVM3Hal NVM3 HAL module
NVM3Lock NVM3 lock module
RTCDRV Real-time Clock Driver
SLEEP Sleep Management Driver
SPIDRV SPIDRV Serial Peripheral Interface Driver
TEMPDRV TEMPDRV Temperature Sensor Driver
UARTDRV UARTDRV Universal Asynchronous Receiver/Transmitter Driver
USTIMER USTIMER Microsecond Delay Timer Driver
EMLIB Low-level peripheral library
ACMP Analog comparator (ACMP) Peripheral API
ADC Analog to Digital Converter (ADC) Peripheral API
ASSERT Error checking module
BUS BUS register and RAM bit/field read/write API
CHIP Chip errata workarounds initialization API
CMU Clock management unit (CMU) Peripheral API
COMMON General purpose utilities and cross-compiler support
CORE Core interrupt handling API
CRYOTIMER Ultra Low Energy Timer/Counter (CRYOTIMER) Peripheral API
CRYPTO Cryptography accelerator peripheral API
DBG Debug (DBG) Peripheral API
EMU Energy Management Unit (EMU) Peripheral API
GPCRC General Purpose Cyclic Redundancy Check (GPCRC) API
GPIO General Purpose Input/Output (GPIO) API
I2C Inter-integrated Circuit (I2C) Peripheral API
IDAC Current Digital-to-Analog Converter (IDAC) Peripheral API
INT Safe nesting of interrupt disable/enable API
LDMA Linked Direct Memory Access (LDMA) Peripheral API
LETIMER Low Energy Timer (LETIMER) Peripheral API
LEUART Low Energy Universal Asynchronous Receiver/Transmitter (LEUART) Peripheral API
MPU Memory Protection Unit (MPU) Peripheral API
MSC Memory System Controller API
PCNT Pulse Counter (PCNT) Peripheral API
PRS Peripheral Reflex System (PRS) Peripheral API
RAMFUNC RAM code support
RMU Reset Management Unit (RMU) Peripheral API
RTCC Real Time Counter (RTCC) Peripheral API
SYSTEM System API
TIMER Timer/Counter (TIMER) Peripheral API
USART Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API
VERSION Version API
WDOG Watchdog (WDOG) Peripheral API
External Device Drivers External Device Drivers is a collection of device drivers for external components. These components are typically Silicon Laboratories ICs that are not part of the Gecko families of SoCs
EFP Driver EFP (Energy Friendly PMIC) driver
Kit Drivers Kit support and drivers
CPT112S_I2C Silicon Labs 12-pad Capacitive Touch Evaluation Board I2C driver
CapSense Capacitive sensing driver
Display Display device driver stack library
DmaCtrl UDMA control block array
EEPROM I2C EEPROM Driver
Gecko USB MSD USB Mass Storage Class (MSC)
Gecko USB RS232 bridge Gecko USB to RS232 bridge (CDC Class)
HidKeyboard Implements a USB HID class keyboard
I2CSPM I2C Simple Polled Master driver
Ksz8851snl KSZ8851SNL SPI Ethernet Controller driver
MicroSd SPI driver for micro SD card
NANDFlash Driver for Numonyx NAND256W3A NAND Flash devices
NORFlash Driver for Spanion S29GL128P90FFIR13 and S29GL064N NOR Flash devices
RetargetIo Standard I/O retargeting driver
SegmentLcd Segment LCD driver
Si114x Silicon Labs Si114x Ultraviolet (UV) Index, Gesture, Proximity, and Ambient Light Sensor I2C driver
Si7013 Silicon Labs Si7013 Relative Humidity and Temperature Sensor I2C driver
Si72xx Silicon Labs Si72xx Magnetic Hall Effect Sensor I2C driver
TFT Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode
TempSensor Driver for DS75 I2C temperature sensor
Textdisplay Line based text output terminal interface on top of the DISPLAY device driver stack. See TextDisplay Library for more information
Touch Touch panel driver for DK3650, DK3750 and DK3850 Development Kits
Udelay Calibrated busy wait loop
UsbHid USB HID keyboard scan codes
VddCheck VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API
Platform Common Gecko Platform Common components are used throughout the Gecko SDK
BIT
SLIST
Status Codes
Platform Middleware Gecko Platform Middleware for use with EFM32, EZR32 and EFR32 products
Capacitive Sensing Firmware Library Capacitive sensing firmware library for Silicon Labs MCUs
GLIB Graphics Library
Platform Services Gecko Platform Service components are high-level, device-independent and thread-safe APIs. Each service may have a hardware abstraction layer (HAL)
MPU MPU basic utilities
SLEEPTIMER Low frequency timer utilities. Utilities (timer, delays and time keeping)