WDOG_Init_TypeDef Struct Reference

Watchdog initialization structure.

Definition at line 130 of file em_wdog.h.

#include <em_wdog.h>

Data Fields

WDOG_ClkSel_TypeDef clkSel
 
bool debugRun
 
bool em2Run
 
bool em3Run
 
bool em4Block
 
bool enable
 
bool lock
 
WDOG_PeriodSel_TypeDef perSel
 
bool resetDisable
 
bool swoscBlock
 
WDOG_WarnSel_TypeDef warnSel
 
WDOG_WinSel_TypeDef winSel
 

Field Documentation

WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel

Clock source to use for watchdog.

Definition at line 156 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::debugRun

Counter keeps running during debug halt.

Definition at line 135 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::em2Run

Counter keeps running when in EM2.

Definition at line 138 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::em3Run

Counter keeps running when in EM3.

Definition at line 141 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::em4Block

Block EMU from entering EM4.

Definition at line 144 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::enable

Enable watchdog when initialization completed.

Definition at line 132 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::lock

Block SW from modifying the configuration (a reset is needed to reconfigure).

Definition at line 152 of file em_wdog.h.

Referenced by WDOGn_Init().

WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel

Watchdog timeout period.

Definition at line 160 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::resetDisable

Disable watchdog reset output if true

Definition at line 177 of file em_wdog.h.

Referenced by WDOGn_Init().

bool WDOG_Init_TypeDef::swoscBlock

Block SW from disabling LFRCO/LFXO oscillators.

Definition at line 148 of file em_wdog.h.

Referenced by WDOGn_Init().

WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel

Select warning time as % of the watchdog timeout

Definition at line 165 of file em_wdog.h.

Referenced by WDOGn_Init().

WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel

Select illegal window time as % of the watchdog timeout

Definition at line 171 of file em_wdog.h.

Referenced by WDOGn_Init().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_wdog.h