__HALL_Config Struct Reference

Structure to configure the Hall effect sensor device.

Definition at line 67 of file hall.h.

#include <hall.h>

Data Fields

float hysteresis
 
bool outputInvert
 
uint8_t polarity
 
float threshold
 

Field Documentation

float __HALL_Config::hysteresis

Hysteresis in mT

Definition at line 69 of file hall.h.

Referenced by HALL_configure().

bool __HALL_Config::outputInvert

The polarity of the output pin

Definition at line 71 of file hall.h.

Referenced by HALL_configure().

uint8_t __HALL_Config::polarity

Magnetic field polarity setting

Definition at line 70 of file hall.h.

Referenced by HALL_configure().

float __HALL_Config::threshold

Decision point for magnetic field high or low in mT

Definition at line 68 of file hall.h.

Referenced by HALL_configure().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/bsp/thunderboard/hall.h