EZRADIODRV_HandleData Struct Reference
EzRadio driver instance initialization and handler structure. This data structure contains a number of EzRadio driver configuration options. Handler to this structure is passed to ezradioInit() when initializing an EzRadio driver instance. Some common initialization data sets are predefined in EZRADIODRV_INIT_DEFAULT. Note: All the referenced plug-in instances has there own handler sturcture, that is referenced from this structure.
Definition at line 299
of file ezradio_plugin_manager.h
.
#include <
ezradio_plugin_manager.h
>
Data Fields | |
EZRADIODRV_AutoAckHandle_t | autoAck |
Auto-acknowledge plug-in handler. | |
EZRADIODRV_DirectRxHandle_t | directRx |
Direct reception plug-in handler. | |
EZRADIODRV_DirectTxHandle_t | directTx |
Direct transmission plug-in handler. | |
EZRADIODRV_PacketCrcErrorHandle_t | packetCrcError |
Packet reception with CRC error plug-in handler. | |
EZRADIODRV_PacketRxHandle_t | packetRx |
Packet reception plug-in handler. | |
EZRADIODRV_PacketTxHandle_t | packetTx |
Packet transmission plug-in handler. | |
EZRADIODRV_Pn9Handle_t | pn9 |
PN9 plug-in handler. | |
EZRADIODRV_UnmodCarrierHandle_t | unmodCarrier |
Unmodulated carrier plug-in handler. | |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emdrv/ezradiodrv/plugins/inc/
ezradio_plugin_manager.h