BATTERY_TypeDef Struct Reference
Defines segment COM and BIT fields for Battery (suited for Anim)
Definition at line 128
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [4] |
uint8_t | com [4] |
Field Documentation
uint8_t BATTERY_TypeDef::bit[4] |
uint8_t BATTERY_TypeDef::com[4] |
LCD COM line (for multiplexing)
Definition at line 129
of file segmentlcd.c
.
Referenced by SegmentLCD_Battery().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/drivers/
segmentlcd.c