LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.
Definition at line 238
of file uartdrv.h
.
#include <
uartdrv.h
>
Data Fields | |
uint32_t | baudRate |
UART baud rate. | |
uint8_t | ctsPin |
CTS pin number. | |
GPIO_Port_TypeDef | ctsPort |
CTS pin port number. | |
UARTDRV_FlowControlType_t | fcType |
Flow control mode. | |
LEUART_Parity_TypeDef | parity |
Parity configuration. | |
LEUART_TypeDef * | port |
The peripheral used for LEUART. | |
uint8_t | portLocation |
Location number for LEUART pins. | |
uint8_t | rtsPin |
RTS pin number. | |
GPIO_Port_TypeDef | rtsPort |
RTS pin port number. | |
UARTDRV_Buffer_FifoQueue_t * | rxQueue |
Receive operation queue. | |
LEUART_Stopbits_TypeDef | stopBits |
Number of stop bits. | |
UARTDRV_Buffer_FifoQueue_t * | txQueue |
Transmit operation queue. | |
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emdrv/uartdrv/inc/
uartdrv.h