sl_sleeptimer_timer_handle Struct Reference

Definition at line 63 of file sl_sleeptimer.h .

Data Fields

sl_sleeptimer_timer_callback_t callback
Function to call when timer expires.
void * callback_data
User data to pass to callback function.
uint32_t delta
Delay relative to previous element in list.
sl_sleeptimer_timer_handle_t * next
Pointer to next element in list.
uint16_t option_flags
Option flags.
uint8_t priority
Priority of timer.
uint32_t timeout_periodic
Periodic timeout.

The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/service/sleeptimer/inc/ sl_sleeptimer.h