rtcdriver.c File Reference
RTCDRV timer API implementation.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
Definition in file rtcdriver.c
.
#include <string.h>
#include "em_device.h"
#include "em_cmu.h
"
#include "em_common.h
"
#include "em_core.h
"
#include "em_rtcc.h
"
#include "rtcdriver.h
"
Functions | |
Ecode_t | RTCDRV_AllocateTimer (RTCDRV_TimerID_t *id) |
Allocate timer. | |
Ecode_t | RTCDRV_DeInit (void) |
Deinitialize the RTCDRV driver. | |
Ecode_t | RTCDRV_Delay (uint32_t ms) |
Millisecond delay function. | |
Ecode_t | RTCDRV_FreeTimer (RTCDRV_TimerID_t id) |
Free timer. | |
uint32_t | RTCDRV_GetWallClock (void) |
Get wallclock time. | |
uint32_t | RTCDRV_GetWallClockTicks32 (void) |
Get wallclock tick count as a 32bit value. At 4 ticks per millisecond, overflow occurs after approximately 12.5 days. | |
uint64_t | RTCDRV_GetWallClockTicks64 (void) |
Get a wallclock tick count as a 64 bit value. | |
Ecode_t | RTCDRV_Init (void) |
Initialize the RTCDRV driver. | |
Ecode_t | RTCDRV_IsRunning (RTCDRV_TimerID_t id, bool *isRunning) |
Check if a given timer is running. | |
uint64_t | RTCDRV_MsecsToTicks (uint32_t ms) |
Convert from milliseconds to RTC/RTCC ticks. | |
uint64_t | RTCDRV_SecsToTicks (uint32_t secs) |
Convert from seconds to RTC/RTCC ticks. | |
Ecode_t | RTCDRV_SetWallClock (uint32_t secs) |
Set wallclock time. | |
Ecode_t | RTCDRV_StartTimer (RTCDRV_TimerID_t id, RTCDRV_TimerType_t type, uint32_t timeout, RTCDRV_Callback_t callback, void *user) |
Start a timer. | |
Ecode_t | RTCDRV_StopTimer (RTCDRV_TimerID_t id) |
Stop a given timer. | |
uint32_t | RTCDRV_TicksToMsec (uint64_t ticks) |
Convert from RTC/RTCC ticks to milliseconds. | |
uint64_t | RTCDRV_TicksToMsec64 (uint64_t ticks) |
Convert from RTC/RTCC ticks to milliseconds with 64-bit resolution. | |
uint32_t | RTCDRV_TicksToSec (uint64_t ticks) |
Convert from RTC/RTCC ticks to seconds. | |
Ecode_t | RTCDRV_TimeRemaining (RTCDRV_TimerID_t id, uint32_t *timeRemaining) |
Get time left before a given timer expires. | |