Scan sequence initialization structure.
Definition at line 863
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
bool | fifoOverwrite |
bool | leftAdjust |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
bool | scanDmaEm2Wu |
ADC_InitScanInput_TypeDef | scanInputConfig |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line 871
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::diff |
Select if single-ended or differential input.
Definition at line 901
of file em_adc.h
.
Referenced by ADC_InitScan(), ADC_ScanDifferentialInputAdd(), and ADC_ScanSingleEndedInputAdd().
bool ADC_InitScan_TypeDef::fifoOverwrite |
When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.
Definition at line 920
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line 907
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line 904
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsEnable
is enabled.
Definition at line 868
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
Definition at line 877
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line 910
of file em_adc.h
.
Referenced by ADC_InitScan().
ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
bool ADC_InitScan_TypeDef::scanDmaEm2Wu |
When true, DMA is available in EM2 for scan conversion
Definition at line 914
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig |
Scan input configuration. Use ADC_ScanInputClear(), ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this structure.
Definition at line 897
of file em_adc.h
.
Referenced by ADC_InitScan(), ADC_ScanDifferentialInputAdd(), ADC_ScanInputClear(), and ADC_ScanSingleEndedInputAdd().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_adc.h