Transmit_Plugin
Detailed Description
Transmit plugin, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
| struct | EZRADIODRV_FieldLength |
| struct | EZRADIODRV_PacketLengthConfig |
|
EzRadio transmit packet length configuration structure.
|
|
| struct | EZRADIODRV_PacketTxHandle |
|
EzRadio transmit plug-in instance initialization and handler structure.
|
|
Macros |
|
| #define | ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED ( ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE | 0x00000001) |
|
Unable to start transmission.
|
|
| #define | EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT |
|
Configuration data for EzRadio transmit plug-in.
|
|
Typedefs |
|
| typedef struct EZRADIODRV_FieldLength | EZRADIODRV_FieldLength_t |
| typedef struct EZRADIODRV_PacketLengthConfig | EZRADIODRV_PacketLengthConfig_t |
|
EzRadio transmit packet length configuration structure.
|
|
| typedef struct EZRADIODRV_PacketTxHandle | EZRADIODRV_PacketTxHandle_t |
|
EzRadio transmit plug-in instance initialization and handler structure.
|
|
| typedef enum EZRADIODRV_TransmitLengthMode | EZRADIODRV_TransmitLengthMode_t |
|
EzRadio transmit packet length mode.
|
|
| typedef enum EZRADIODRV_TransmitPacketType | EZRADIODRV_TransmitPacketType_t |
|
EzRadio transmit packet type.
|
|
Enumerations |
|
| enum |
EZRADIODRV_TransmitLengthMode
{
ezradiodrvTransmitLenghtDefault = 0, ezradiodrvTransmitLenghtCustomPacketLen = 1, ezradiodrvTransmitLenghtCustomFieldLen = 2 } |
|
EzRadio transmit packet length mode.
|
|
| enum |
EZRADIODRV_TransmitPacketType
{
ezradiodrvPacketTypeNormal = 0, ezradiodrvPacketTypeAutoAck = 1 } |
|
EzRadio transmit packet type.
|
|
Functions |
|
| Ecode_t | ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle, uint16_t packetLength, uint8_t *pioRadioPacket) |
|
Start basic transmission. Radio transmits with data only in the first field in this case.
|
|
| Ecode_t | ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
|
Start transmission using the packet parameters from the generated configuration header file.
|
|
| Ecode_t | ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
|
Start transmission using the packet parameters from pktLengthConf.
|
|
| Ecode_t | ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) |
|
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
|
|
| Ecode_t | ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) |
|
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.
|
|
Macro Definition Documentation
| #define EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio transmit plug-in.
Definition at line
114
of file
ezradio_transmit_plugin.h
.
Typedef Documentation
| typedef struct EZRADIODRV_FieldLength EZRADIODRV_FieldLength_t |
EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.
Enumeration Type Documentation
EzRadio transmit packet length mode.
Definition at line
66
of file
ezradio_transmit_plugin.h
.
Function Documentation
| Ecode_t ezradioStartTransmitBasic | ( | EZRADIODRV_Handle_t |
radioHandle,
|
| uint16_t |
packetLength,
|
||
| uint8_t * |
pioRadioPacket
|
||
| ) |
Start basic transmission. Radio transmits with data only in the first field in this case.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet length and channel configurations are set. packetLengthLength of the basic packet. pioRadioPacketPointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
68
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
| Ecode_t ezradioStartTransmitConfigured | ( | EZRADIODRV_Handle_t |
radioHandle,
|
| uint8_t * |
pioRadioPacket
|
||
| ) |
Start transmission using the packet parameters from the generated configuration header file.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet length and channel configurations are set. pioRadioPacketPointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
109
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtDefault , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
| Ecode_t ezradioStartTransmitCustom | ( | EZRADIODRV_Handle_t |
radioHandle,
|
| EZRADIODRV_PacketLengthConfig_t |
pktLengthConf,
|
||
| uint8_t * |
pioRadioPacket
|
||
| ) |
Start transmission using the packet parameters from pktLengthConf.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet length and channel configurations are set. pktLengthConfPacket length configuration structure configuration of the custom packet. pioRadioPacketPointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
150
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitSmart() .
| Ecode_t ezradioStartTransmitDefault | ( | EZRADIODRV_Handle_t |
radioHandle,
|
| uint8_t * |
pioRadioPacket
|
||
| ) |
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet length and channel configurations are set. pioRadioPacketPointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
219
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradioStartTransmitSmart() , EZRADIODRV_PacketTxHandle::lenConfig , and EZRADIODRV_HandleData::packetTx .
| Ecode_t ezradioStartTransmitSmart | ( | EZRADIODRV_Handle_t |
radioHandle,
|
| EZRADIODRV_PacketLengthConfig_t |
pktLengthConf,
|
||
| uint8_t * |
pioRadioPacket
|
||
| ) |
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.
- Parameters
-
radioHandleHandler of the EzRadio driver instance where packet length and channel configurations are set. pktLengthConfPacket length configuration structure configuration of the custom packet. pioRadioPacketPointer to the packet buffer.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line
189
of file
ezradio_transmit_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomFieldLen , ezradiodrvTransmitLenghtCustomPacketLen , ezradiodrvTransmitLenghtDefault , ezradioStartTransmitBasic() , ezradioStartTransmitConfigured() , ezradioStartTransmitCustom() , EZRADIODRV_PacketLengthConfig::lenMode , and EZRADIODRV_PacketLengthConfig::pktLen .
Referenced by ezradioStartTransmitDefault() .