__GLIB_Font_t Struct Reference
Font definition structure.
Definition at line
224
of file
glib.h
.
#include <
glib.h
>
Data Fields |
|
| uint8_t | charSpacing |
| GLIB_Font_Class | class |
| uint16_t | cntOfMapElements |
| uint8_t | fontHeight |
| uint8_t | fontRowOffset |
| uint8_t | fontWidth |
| uint8_t | lineSpacing |
| void * | pFontPixMap |
| uint8_t | sizeOfMapElement |
Field Documentation
| uint8_t __GLIB_Font_t::charSpacing |
Number of pixels between each character in this font.
Definition at line
247
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| GLIB_Font_Class __GLIB_Font_t::class |
The font class is used to tell glib if the font contains numbers only or characters and numbers
Definition at line
251
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint16_t __GLIB_Font_t::cntOfMapElements |
Number of elements in the font pixel map.
Definition at line
229
of file
glib.h
.
Referenced by GLIB_drawChar() .
| uint8_t __GLIB_Font_t::fontHeight |
Height in pixels of each character.
Definition at line
241
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint8_t __GLIB_Font_t::fontRowOffset |
| uint8_t __GLIB_Font_t::fontWidth |
Width in pixels of each character.
Definition at line
238
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint8_t __GLIB_Font_t::lineSpacing |
Number of pixels between each line in this font.
Definition at line
244
of file
glib.h
.
Referenced by GLIB_drawString() .
| void* __GLIB_Font_t::pFontPixMap |
Pointer to the pixel map for the font.
Definition at line
226
of file
glib.h
.
Referenced by GLIB_drawChar() .
| uint8_t __GLIB_Font_t::sizeOfMapElement |
Size of each element in the font pixel map.
Definition at line
232
of file
glib.h
.
Referenced by GLIB_drawChar() .
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/middleware/glib/glib/
glib.h