__BMP_Header Struct Reference
BMP Module header structure. Must be packed to exact 54 bytes.
Definition at line
86
of file
bmp.h
.
#include <
bmp.h
>
Data Fields |
|
| uint16_t | bitsPerPixel |
| uint16_t | colorPlanes |
| uint32_t | colorsRequired |
| uint32_t | colorsUsed |
| uint32_t | compressionType |
| uint32_t | dataOffset |
| uint32_t | fileSize |
| uint32_t | headerSize |
| uint32_t | height |
| uint32_t | hPixelsPerMeter |
| uint32_t | imageDataSize |
| uint16_t | magic |
| uint16_t | reserved1 |
| uint16_t | reserved2 |
| uint32_t | vPixelsPerMeter |
| uint32_t | width |
Field Documentation
| uint16_t __BMP_Header::bitsPerPixel |
Color depth
Definition at line
110
of file
bmp.h
.
Referenced by BMP_getBitsPerPixel() , BMP_readRawData() , BMP_readRgbData() , and BMP_reset() .
| uint16_t __BMP_Header::colorPlanes |
Color planes
Definition at line
108
of file
bmp.h
.
| uint32_t __BMP_Header::colorsRequired |
Number of color indices that are required for displaying the bitmap
Definition at line
122
of file
bmp.h
.
| uint32_t __BMP_Header::colorsUsed |
Number of color indices in the color table that are actually used by the bitmap
Definition at line
120
of file
bmp.h
.
| uint32_t __BMP_Header::compressionType |
Compression type
Definition at line
112
of file
bmp.h
.
Referenced by BMP_getCompressionType() , BMP_readRawData() , BMP_readRgbData() , and BMP_reset() .
| uint32_t __BMP_Header::dataOffset |
Data offset relative to the start of the bmp data
Definition at line
100
of file
bmp.h
.
Referenced by BMP_getDataOffset() , and BMP_reset() .
| uint32_t __BMP_Header::fileSize |
Size of the bmp file in bytes
Definition at line
94
of file
bmp.h
.
Referenced by BMP_getFileSize() , and BMP_reset() .
| uint32_t __BMP_Header::headerSize |
| uint32_t __BMP_Header::height |
Height of bmp
Definition at line
106
of file
bmp.h
.
Referenced by BMP_getHeight() , BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRgbData() , and BMP_reset() .
| uint32_t __BMP_Header::hPixelsPerMeter |
Horizontal resolution (pixels per meter)
Definition at line
116
of file
bmp.h
.
| uint32_t __BMP_Header::imageDataSize |
Size of raw BMP data
Definition at line
114
of file
bmp.h
.
Referenced by BMP_getImageDataSize() , BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRgbData() , and BMP_reset() .
| uint16_t __BMP_Header::magic |
Magic identifier: "BM" (for bmp files)
Definition at line
92
of file
bmp.h
.
Referenced by BMP_reset() .
| uint16_t __BMP_Header::reserved1 |
Reserved 1
Definition at line
96
of file
bmp.h
.
| uint16_t __BMP_Header::reserved2 |
Reserved 2
Definition at line
98
of file
bmp.h
.
| uint32_t __BMP_Header::vPixelsPerMeter |
Vertical resolution (pixels per meter)
Definition at line
118
of file
bmp.h
.
| uint32_t __BMP_Header::width |
Width of bmp
Definition at line
104
of file
bmp.h
.
Referenced by BMP_getWidth() , BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , and BMP_readRgbData() .
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/middleware/glib/glib/
bmp.h