uartdrv.c File Reference
UARTDRV API implementation.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
Definition in file
uartdrv.c
.
#include <string.h>
#include "
uartdrv.h
"
#include "em_device.h"
#include "
em_emu.h
"
#include "
em_gpio.h
"
#include "
em_core.h
"
#include "
gpiointerrupt.h
"
Functions |
|
| Ecode_t | UARTDRV_Abort ( UARTDRV_Handle_t handle, UARTDRV_AbortType_t type) |
|
Abort ongoing UART transfers.
|
|
| Ecode_t | UARTDRV_DeInit ( UARTDRV_Handle_t handle) |
|
Deinitialize a UART driver instance.
|
|
| UARTDRV_FlowControlState_t | UARTDRV_FlowControlGetPeerStatus ( UARTDRV_Handle_t handle) |
|
Check the peer's flow control status.
|
|
| UARTDRV_FlowControlState_t | UARTDRV_FlowControlGetSelfStatus ( UARTDRV_Handle_t handle) |
|
Check the self flow control status.
|
|
| Ecode_t | UARTDRV_FlowControlIgnoreRestrain ( UARTDRV_Handle_t handle) |
|
Enable transmission when restrained by flow control.
|
|
| Ecode_t | UARTDRV_FlowControlSet ( UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state) |
|
Set UART flow control state. Set nRTS pin if hardware flow control is enabled. Send XON/XOFF if software flow control is enabled.
|
|
| Ecode_t | UARTDRV_FlowControlSetPeerStatus ( UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state) |
|
Set peer UART flow control state. Pause/resume transmit accordingly. Only for manual software flow control.
|
|
| UARTDRV_Count_t | UARTDRV_ForceReceive ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t maxCount) |
|
Direct receive without interrupts or callback. This is a blocking function.
|
|
| Ecode_t | UARTDRV_ForceTransmit ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) |
|
Direct transmit without interrupts or callback. This is a blocking function. that ignores flow control if enabled.
|
|
| UARTDRV_Status_t | UARTDRV_GetPeripheralStatus ( UARTDRV_Handle_t handle) |
|
Return the status of the UART peripheral associated with a given handle.
|
|
| uint8_t | UARTDRV_GetReceiveDepth ( UARTDRV_Handle_t handle) |
|
Return the number of queued receive operations.
|
|
| UARTDRV_Status_t | UARTDRV_GetReceiveStatus ( UARTDRV_Handle_t handle, uint8_t **buffer, UARTDRV_Count_t *itemsReceived, UARTDRV_Count_t *itemsRemaining) |
|
Check the status of the UART and gather information about any ongoing receive operations.
|
|
| uint8_t | UARTDRV_GetTransmitDepth ( UARTDRV_Handle_t handle) |
|
Returns the number of queued transmit operations.
|
|
| UARTDRV_Status_t | UARTDRV_GetTransmitStatus ( UARTDRV_Handle_t handle, uint8_t **buffer, UARTDRV_Count_t *itemsSent, UARTDRV_Count_t *itemsRemaining) |
|
Check the status of the UART and gather information about any ongoing transmit operations.
|
|
| Ecode_t | UARTDRV_InitLeuart ( UARTDRV_Handle_t handle, const UARTDRV_InitLeuart_t *initData) |
|
Initialize a LEUART driver instance.
|
|
| Ecode_t | UARTDRV_InitUart ( UARTDRV_Handle_t handle, const UARTDRV_InitUart_t *initData) |
|
Initialize a U(S)ART driver instance.
|
|
| Ecode_t | UARTDRV_PauseTransmit ( UARTDRV_Handle_t handle) |
|
Pause an ongoing transmit operation.
|
|
| Ecode_t | UARTDRV_Receive ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count, UARTDRV_Callback_t callback) |
|
Start a non-blocking receive.
|
|
| Ecode_t | UARTDRV_ReceiveB ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) |
|
Start a blocking receive.
|
|
| Ecode_t | UARTDRV_ResumeTransmit ( UARTDRV_Handle_t handle) |
|
Resume a paused transmit operation.
|
|
| Ecode_t | UARTDRV_Transmit ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count, UARTDRV_Callback_t callback) |
|
Start a non-blocking transmit.
|
|
| Ecode_t | UARTDRV_TransmitB ( UARTDRV_Handle_t handle, uint8_t *data, UARTDRV_Count_t count) |
|
Start a blocking transmit.
|
|