HFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
Definition at line 559
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
uint8_t | coreBiasAna |
uint8_t | coreBiasStartup |
CMU_HfxoCoreDegen_TypeDef | coreDegenAna |
CMU_HfxoCtuneFixCap_TypeDef | ctuneFixAna |
uint8_t | ctuneXiAna |
uint8_t | ctuneXiStartup |
uint8_t | ctuneXoAna |
uint8_t | ctuneXoStartup |
bool | disOnDemand |
bool | enXiDcBiasAna |
bool | forceEn |
bool | forceXi2GndAna |
bool | forceXo2GndAna |
uint8_t | imCoreBiasStartup |
CMU_HfxoOscMode_TypeDef | mode |
bool | regLock |
CMU_HfxoCbLsbTimeout_TypeDef | timeoutCbLsb |
CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteady |
CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteadyFirstLock |
Field Documentation
uint8_t CMU_HFXOInit_TypeDef::coreBiasAna |
uint8_t CMU_HFXOInit_TypeDef::coreBiasStartup |
CMU_HfxoCoreDegen_TypeDef CMU_HFXOInit_TypeDef::coreDegenAna |
CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna |
Fixed tuning capacitance on XI/XO.
Definition at line 568
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
uint8_t CMU_HFXOInit_TypeDef::ctuneXiAna |
Tuning capacitance on XI.
Definition at line 570
of file em_cmu.h
.
Referenced by BSP_initClocks(), and CMU_HFXOInit().
uint8_t CMU_HFXOInit_TypeDef::ctuneXiStartup |
XI pin startup tuning capacitance.
Definition at line 564
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
uint8_t CMU_HFXOInit_TypeDef::ctuneXoAna |
Tuning capacitance on XO.
Definition at line 569
of file em_cmu.h
.
Referenced by BSP_initClocks(), and CMU_HFXOInit().
uint8_t CMU_HFXOInit_TypeDef::ctuneXoStartup |
XO pin startup tuning capacitance.
Definition at line 563
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
bool CMU_HFXOInit_TypeDef::disOnDemand |
bool CMU_HFXOInit_TypeDef::enXiDcBiasAna |
bool CMU_HFXOInit_TypeDef::forceEn |
bool CMU_HFXOInit_TypeDef::forceXi2GndAna |
bool CMU_HFXOInit_TypeDef::forceXo2GndAna |
uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup |
Core bias intermediate startup current.
Definition at line 566
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
CMU_HfxoOscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
bool CMU_HFXOInit_TypeDef::regLock |
CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb |
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady |
Steady state timeout duration.
Definition at line 562
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock |
Steady state timeout duration for first lock.
Definition at line 561
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_cmu.h