SMU_PrivilegedAccess_TypeDef Struct Reference

SMU peripheral privileged access enablers.

Definition at line 484 of file em_smu.h.

#include <em_smu.h>

Data Fields

bool privilegedACMP0: 1
 
bool privilegedACMP1: 1
 
bool privilegedAHBRADIO: 1
 
bool privilegedAMUXCP0: 1
 
bool privilegedBUFC: 1
 
bool privilegedBURAM: 1
 
bool privilegedBURTC: 1
 
bool privilegedCHIPTESTCTRL: 1
 
bool privilegedCMU: 1
 
bool privilegedDPLL0: 1
 
bool privilegedEMU: 1
 
bool privilegedFSRCO: 1
 
bool privilegedGPCRC: 1
 
bool privilegedGPIO: 1
 
bool privilegedHFRCO0: 1
 
bool privilegedHFRCOEM23: 1
 
bool privilegedHFXO0: 1
 
bool privilegedI2C0: 1
 
bool privilegedI2C1: 1
 
bool privilegedIADC0: 1
 
bool privilegedICACHE0: 1
 
bool privilegedIFADCDEBUG: 1
 
bool privilegedLDMA: 1
 
bool privilegedLDMAXBAR: 1
 
bool privilegedLETIMER0: 1
 
bool privilegedLFRCO: 1
 
bool privilegedLFXO: 1
 
bool privilegedLVGD: 1
 
bool privilegedMSC: 1
 
bool privilegedPRS: 1
 
bool privilegedRADIOAES: 1
 
bool privilegedReserved0: 1
 
bool privilegedRTCC: 1
 
bool privilegedSEMAILBOX: 1
 
bool privilegedSMU: 1
 
bool privilegedSYSCFG: 1
 
bool privilegedTIMER0: 1
 
bool privilegedTIMER1: 1
 
bool privilegedTIMER2: 1
 
bool privilegedTIMER3: 1
 
bool privilegedULFRCO: 1
 
bool privilegedUSART0: 1
 
bool privilegedUSART1: 1
 
bool privilegedUSART2: 1
 
bool privilegedWDOG0: 1
 
bool privilegedWDOG1: 1
 

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0

Definition at line 827 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1

Definition at line 828 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedAHBRADIO

Privileged access enabler for AHBRADIO

Definition at line 837 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedAMUXCP0

Privileged access enabler for AMUXCP0

Definition at line 833 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedBUFC

Privileged access enabler for BUFC

Definition at line 835 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedBURAM

Privileged access enabler for BURAM

Definition at line 820 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedBURTC

Privileged access enabler for BURTC

Definition at line 815 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCHIPTESTCTRL

Privileged access enabler for CHIPTESTCTRL

Definition at line 817 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU

Definition at line 794 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedDPLL0

Privileged access enabler for DPLL0

Definition at line 798 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU

Definition at line 793 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedFSRCO

Privileged access enabler for FSRCO

Definition at line 797 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC

Definition at line 822 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO

Definition at line 805 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedHFRCO0

Privileged access enabler for HFRCO0

Definition at line 796 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedHFRCOEM23

Privileged access enabler for HFRCOEM23

Definition at line 830 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedHFXO0

Privileged access enabler for HFXO0

Definition at line 795 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0

Definition at line 829 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C1

Privileged access enabler for I2C1

Definition at line 816 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedIADC0

Privileged access enabler for IADC0

Definition at line 826 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedICACHE0

Privileged access enabler for ICACHE0

Definition at line 803 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedIFADCDEBUG

Privileged access enabler for IFADCDEBUG

Definition at line 821 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA

Definition at line 806 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMAXBAR

Privileged access enabler for LDMAXBAR

Definition at line 807 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER

Definition at line 825 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLFRCO

Privileged access enabler for LFRCO

Definition at line 800 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLFXO

Privileged access enabler for LFXO

Definition at line 799 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLVGD

Privileged access enabler for LVGD

Definition at line 818 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MSC

Definition at line 802 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS

Definition at line 804 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRADIOAES

Privileged access enabler for RADIOAES

Definition at line 834 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC

Definition at line 823 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSEMAILBOX

Privileged access enabler for SEMAILBOX

Definition at line 838 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU

Definition at line 836 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSYSCFG

Privileged access enabler for SYSCFG

Definition at line 819 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0

Definition at line 808 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1

Definition at line 809 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER2

Privileged access enabler for TIMER2

Definition at line 810 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER3

Privileged access enabler for TIMER3

Definition at line 811 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedULFRCO

Privileged access enabler for ULFRCO

Definition at line 801 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0

Definition at line 812 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1

Definition at line 813 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART2

Privileged access enabler for USART2

Definition at line 814 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0

Definition at line 831 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG1

Privileged access enabler for WDOG1

Definition at line 832 of file em_smu.h.


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_smu.h