NUMBER_TypeDef Struct Reference

Defines segment COM and BIT fields numeric display.

Definition at line 104 of file segmentlcd.c.

Data Fields

uint8_t bit [7]
 
uint8_t com [7]
 

Field Documentation

uint8_t NUMBER_TypeDef::bit[7]

LCD bit number

Definition at line 106 of file segmentlcd.c.

uint8_t NUMBER_TypeDef::com[7]

LCD COM line (for multiplexing)

Definition at line 105 of file segmentlcd.c.


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/segmentlcd.c