ezradio_auto_ack_plugin.c File Reference

EzRadio auto acknowledge plug-in managed by the plug-in manager if enabled.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
  3. This notice may not be removed or altered from any source distribution.

Definition in file ezradio_auto_ack_plugin.c .

#include <stddef.h>
#include "em_device.h"
#include "ezradio_cmd.h"
#include "ezradio_prop.h"
#include " ezradio_api_lib.h "
#include "ezradio_api_lib_add.h"
#include " ezradio_plugin_manager.h "

Functions

void ezradioDisableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle)
Disables auto acknowledge sending feature.
void ezradioEnableAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle)
Enables auto acknowledge sending feature.
void ezradioSkipAutoAck ( EZRADIODRV_AutoAckHandle_t *autoAckHandle)
Configures auto acknowledge sending feature so that there will be no acknowledge transmitted to the next received packet. This is usefull is both nodes of a link uses auto acknowledgement.