Synchronous mode initialization structure.
       Definition at line
       
        417
       
       of file
       
        em_usart.h
       
       .
      
      
       #include <
       
     
        em_usart.h
       
       >
      
| Data Fields | |
| bool | autoCsEnable | 
| uint8_t | autoCsHold | 
| uint8_t | autoCsSetup | 
| bool | autoTx | 
| uint32_t | baudrate | 
| USART_ClockMode_TypeDef | clockMode | 
| USART_Databits_TypeDef | databits | 
| USART_Enable_TypeDef | enable | 
| bool | master | 
| bool | msbf | 
| USART_PRS_Channel_t | prsRxCh | 
| bool | prsRxEnable | 
| uint32_t | refFreq | 
Field Documentation
| bool USART_InitSync_TypeDef::autoCsEnable | 
| uint8_t USART_InitSync_TypeDef::autoCsHold | 
Auto CS hold time in baud cycles
        Definition at line
        
         461
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitSync() .
| uint8_t USART_InitSync_TypeDef::autoCsSetup | 
Auto CS setup time in baud cycles
        Definition at line
        
         464
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitSync() .
| bool USART_InitSync_TypeDef::autoTx | 
Enable AUTOTX mode. Transmits as long as RX is not full. Generates underflows if TX is empty.
        Definition at line
        
         453
        
        of file
        
         em_usart.h
        
        .
       
Referenced by MIC_init() , and USART_InitSync() .
| uint32_t USART_InitSync_TypeDef::baudrate | 
Desired baud rate.
        Definition at line
        
         428
        
        of file
        
         em_usart.h
        
        .
       
Referenced by MIC_init() , MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
| USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode | 
Clock polarity/phase mode.
        Definition at line
        
         440
        
        of file
        
         em_usart.h
        
        .
       
Referenced by SPIDRV_Init() , and USART_InitSync() .
| USART_Databits_TypeDef USART_InitSync_TypeDef::databits | 
Number of data bits in frame.
        Definition at line
        
         431
        
        of file
        
         em_usart.h
        
        .
       
Referenced by SPIDRV_Init() , and USART_InitSync() .
| USART_Enable_TypeDef USART_InitSync_TypeDef::enable | 
Specifies whether TX and/or RX shall be enabled when initialization is completed.
        Definition at line
        
         419
        
        of file
        
         em_usart.h
        
        .
       
Referenced by MIC_init() , USART_InitI2s() , and USART_InitSync() .
| bool USART_InitSync_TypeDef::master | 
Select if to operate in master or slave mode.
        Definition at line
        
         434
        
        of file
        
         em_usart.h
        
        .
       
Referenced by SPIDRV_Init() , and USART_InitSync() .
| bool USART_InitSync_TypeDef::msbf | 
Select if to send most or least significant bit first.
        Definition at line
        
         437
        
        of file
        
         em_usart.h
        
        .
       
Referenced by MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
| USART_PRS_Channel_t USART_InitSync_TypeDef::prsRxCh | 
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
        Definition at line
        
         447
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitSync() .
| bool USART_InitSync_TypeDef::prsRxEnable | 
Enable USART Rx via PRS.
        Definition at line
        
         444
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitSync() .
| uint32_t USART_InitSync_TypeDef::refFreq | 
USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.
        Definition at line
        
         425
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitSync() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       em_usart.h