MicroSd
Detailed Description
SPI driver for micro SD card.
Simple micro SD SPI driver with power control and block transfer support.
| Macros | |
| #define | ACMD13 (13 | 0x80) | 
| #define | ACMD23 (23 | 0x80) | 
| #define | ACMD41 (41 | 0x80) | 
| #define | CMD0 (0) | 
| #define | CMD1 (1) | 
| #define | CMD10 (10) | 
| #define | CMD12 (12) | 
| #define | CMD16 (16) | 
| #define | CMD17 (17) | 
| #define | CMD18 (18) | 
| #define | CMD23 (23) | 
| #define | CMD24 (24) | 
| #define | CMD25 (25) | 
| #define | CMD41 (41) | 
| #define | CMD55 (55) | 
| #define | CMD58 (58) | 
| #define | CMD8 (8) | 
| #define | CMD9 (9) | 
| Functions | |
| int | MICROSD_BlockRx (uint8_t *buff, uint32_t btr) | 
| Receive a data block from micro SD card. | |
| int | MICROSD_BlockTx (const uint8_t *buff, uint8_t token) | 
| Send a data block to micro SD card. | |
| void | MICROSD_Deinit (void) | 
| Deinitialize SPI peripheral. Turn off the SPI peripheral and disable SPI GPIO pins. | |
| void | MICROSD_Deselect (void) | 
| Deselect the micro SD card and release the SPI bus. | |
| void | MICROSD_Init (void) | 
| Initialize the SPI peripheral for microSD card usage. SPI pins and speed etc. is defined in microsdconfig.h. | |
| void | MICROSD_PowerOff (void) | 
| Turn off micro SD card power. DK doesn't support socket power control, only disable the SPI clock. | |
| void | MICROSD_PowerOn (void) | 
| Turn on micro SD card power. DK doesn't support socket power control, only enable the SPI clock. | |
| int | MICROSD_Select (void) | 
| Select the micro SD card and wait for the card to become ready. | |
| uint8_t | MICROSD_SendCmd (uint8_t cmd, DWORD arg) | 
| Send a command packet to micro SD card. | |
| void | MICROSD_SpiClkFast (void) | 
| Set SPI clock to maximum frequency. | |
| void | MICROSD_SpiClkSlow (void) | 
| Set SPI clock to a low frequency suitable for initial card initialization. | |
| bool | MICROSD_TimeOutElapsed (void) | 
| Check if timeout value set with
         
          MICROSD_TimeOutSet()
         
         has elapsed. | |
| void | MICROSD_TimeOutSet (uint32_t msec) | 
| Set a timeout value. The timeout value will be decremented towards zero when SPI traffic to/from the micro SD card takes place. Use
         
          MICROSD_TimeOutElapsed()
         
         to check if timeout has elapsed. | |
| uint8_t | MICROSD_XferSpi (uint8_t data) | 
| Do one SPI transfer. | |
Macro Definition Documentation
| #define ACMD13 (13 | 0x80) | 
SD_STATUS (SDC)
        Definition at line
        
         61
        
        of file
        
         microsd.h
        
        .
       
| #define ACMD23 (23 | 0x80) | 
SET_WR_BLK_ERASE_COUNT (SDC)
        Definition at line
        
         66
        
        of file
        
         microsd.h
        
        .
       
| #define ACMD41 (41 | 0x80) | 
SEND_OP_COND (SDC)
        Definition at line
        
         56
        
        of file
        
         microsd.h
        
        .
       
| #define CMD0 (0) | 
| #define CMD1 (1) | 
SEND_OP_COND
        Definition at line
        
         55
        
        of file
        
         microsd.h
        
        .
       
| #define CMD10 (10) | 
SEND_CID
        Definition at line
        
         59
        
        of file
        
         microsd.h
        
        .
       
| #define CMD12 (12) | 
| #define CMD16 (16) | 
SET_BLOCKLEN
        Definition at line
        
         62
        
        of file
        
         microsd.h
        
        .
       
| #define CMD17 (17) | 
READ_SINGLE_BLOCK
        Definition at line
        
         63
        
        of file
        
         microsd.h
        
        .
       
| #define CMD18 (18) | 
READ_MULTIPLE_BLOCK
        Definition at line
        
         64
        
        of file
        
         microsd.h
        
        .
       
| #define CMD23 (23) | 
SET_BLOCK_COUNT
        Definition at line
        
         65
        
        of file
        
         microsd.h
        
        .
       
| #define CMD24 (24) | 
WRITE_BLOCK
        Definition at line
        
         67
        
        of file
        
         microsd.h
        
        .
       
| #define CMD25 (25) | 
WRITE_MULTIPLE_BLOCK
        Definition at line
        
         68
        
        of file
        
         microsd.h
        
        .
       
| #define CMD41 (41) | 
SEND_OP_COND (ACMD)
        Definition at line
        
         69
        
        of file
        
         microsd.h
        
        .
       
| #define CMD55 (55) | 
| #define CMD58 (58) | 
READ_OCR
        Definition at line
        
         71
        
        of file
        
         microsd.h
        
        .
       
| #define CMD8 (8) | 
| #define CMD9 (9) | 
SEND_CSD
        Definition at line
        
         58
        
        of file
        
         microsd.h
        
        .
       
Function Documentation
| int MICROSD_BlockRx | ( | uint8_t * | 
            buff,
            | 
| uint32_t | 
            btr
            | ||
| ) | 
Receive a data block from micro SD card.
- Parameters
- 
         [out] buffData buffer to store received data. btrByte count (must be multiple of 4). 
- Returns
- 1:OK, 0:Failed.
        Definition at line
        
         199
        
        of file
        
         microsd.c
        
        .
       
References MICROSD_XferSpi() .
| int MICROSD_BlockTx | ( | const uint8_t * | 
            buff,
            | 
| uint8_t | 
            token
            | ||
| ) | 
Send a data block to micro SD card.
- Parameters
- 
         [in] buff512 bytes data block to be transmitted. tokenData token. 
- Returns
- 1:OK, 0:Failed.
        Definition at line
        
         268
        
        of file
        
         microsd.c
        
        .
       
References MICROSD_XferSpi() .
| int MICROSD_Select | ( | void | 
            | ) | 
Select the micro SD card and wait for the card to become ready.
- Returns
- 1:Successful, 0:Timeout.
        Definition at line
        
         157
        
        of file
        
         microsd.c
        
        .
       
References MICROSD_Deselect() .
Referenced by MICROSD_PowerOff() , and MICROSD_SendCmd() .
| uint8_t MICROSD_SendCmd | ( | uint8_t | 
            cmd,
            | 
| DWORD | 
            arg
            | ||
| ) | 
Send a command packet to micro SD card.
- Parameters
- 
         [in] cmdCommand byte. [in] argArgument. 
- Returns
- Response value.
        Definition at line
        
         350
        
        of file
        
         microsd.c
        
        .
       
References CMD0 , CMD12 , CMD55 , CMD8 , MICROSD_Deselect() , MICROSD_Select() , and MICROSD_XferSpi() .
| bool MICROSD_TimeOutElapsed | ( | void | 
            | ) | 
Check if timeout value set with MICROSD_TimeOutSet() has elapsed.
- Returns
- True if timeout has elapsed.
        Definition at line
        
         434
        
        of file
        
         microsd.c
        
        .
       
| void MICROSD_TimeOutSet | ( | uint32_t | 
            msec
            | ) | 
Set a timeout value. The timeout value will be decremented towards zero when SPI traffic to/from the micro SD card takes place. Use MICROSD_TimeOutElapsed() to check if timeout has elapsed.
- Parameters
- 
         [in] msecMillisecond timeout value (very approximate). 
        Definition at line
        
         423
        
        of file
        
         microsd.c
        
        .
       
| uint8_t MICROSD_XferSpi | ( | uint8_t | 
            data
            | ) | 
Do one SPI transfer.
- Parameters
- 
         dataByte to transmit. 
- Returns
- Byte received.
        Definition at line
        
         135
        
        of file
        
         microsd.c
        
        .
       
References USART_SpiTransfer() .
Referenced by MICROSD_BlockRx() , MICROSD_BlockTx() , MICROSD_Deselect() , and MICROSD_SendCmd() .