USART
Detailed Description
Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API.
The Universal Synchronous/Asynchronous Receiver/Transmitter (USART) is a very flexible serial I/O module. It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.
The USART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.
Triple buffering and DMA support makes high data-rates possible with minimal CPU intervention. It is possible to transmit and receive large frames while the MCU remains in EM1 Sleep.
This module does not support DMA configuration. The UARTDRV and SPIDRV drivers provide full support for DMA and more.
The following steps are necessary for basic operation:
Clock enable:
To initialize the USART for asynchronous operation (e.g., UART):
To initialize the USART for synchronous operation (e.g., SPI):
After pins are assigned for the application/board, enable pins at the desired location. Available locations can be obtained from the Pin Definitions section in the data sheet.
- Note
- UARTDRV supports all types of UART flow control. Software assisted hardware flow control is available for parts without true UART hardware flow control.
Data Structures | |
struct | USART_InitAsync_TypeDef |
struct | USART_InitI2s_TypeDef |
struct | USART_InitIrDA_TypeDef |
struct | USART_InitSync_TypeDef |
struct | USART_PrsTriggerInit_TypeDef |
Macros | |
#define | USART_INITASYNC_DEFAULT |
#define | USART_INITI2S_DEFAULT |
#define | USART_INITIRDA_DEFAULT |
#define | USART_INITPRSTRIGGER_DEFAULT |
#define | USART_INITSYNC_DEFAULT |
#define | usartIrDAPrsCh0 0U |
#define | usartIrDAPrsCh1 1U |
#define | usartIrDAPrsCh2 2U |
#define | usartIrDAPrsCh3 3U |
#define | usartIrDAPrsCh4 4U |
#define | usartIrDAPrsCh5 5U |
#define | usartIrDAPrsCh6 6U |
#define | usartIrDAPrsCh7 7U |
#define | usartPrsRxCh0 0U |
#define | usartPrsRxCh1 1U |
#define | usartPrsRxCh10 10U |
#define | usartPrsRxCh11 11U |
#define | usartPrsRxCh2 2U |
#define | usartPrsRxCh3 3U |
#define | usartPrsRxCh4 4U |
#define | usartPrsRxCh5 5U |
#define | usartPrsRxCh6 6U |
#define | usartPrsRxCh7 7U |
#define | usartPrsRxCh8 8U |
#define | usartPrsRxCh9 9U |
#define | usartPrsTriggerCh0 0U |
#define | usartPrsTriggerCh1 1U |
#define | usartPrsTriggerCh2 2U |
#define | usartPrsTriggerCh3 3U |
#define | usartPrsTriggerCh4 4U |
#define | usartPrsTriggerCh5 5U |
#define | usartPrsTriggerCh6 6U |
#define | usartPrsTriggerCh7 7U |
Typedefs | |
typedef uint8_t | USART_PRS_Channel_t |
Enumerations | |
enum | USART_ClockMode_TypeDef { usartClockMode0 = USART_CTRL_CLKPOL_IDLELOW | USART_CTRL_CLKPHA_SAMPLELEADING, usartClockMode1 = USART_CTRL_CLKPOL_IDLELOW | USART_CTRL_CLKPHA_SAMPLETRAILING, usartClockMode2 = USART_CTRL_CLKPOL_IDLEHIGH | USART_CTRL_CLKPHA_SAMPLELEADING, usartClockMode3 = USART_CTRL_CLKPOL_IDLEHIGH | USART_CTRL_CLKPHA_SAMPLETRAILING } |
enum | USART_Databits_TypeDef { usartDatabits4 = USART_FRAME_DATABITS_FOUR, usartDatabits5 = USART_FRAME_DATABITS_FIVE, usartDatabits6 = USART_FRAME_DATABITS_SIX, usartDatabits7 = USART_FRAME_DATABITS_SEVEN, usartDatabits8 = USART_FRAME_DATABITS_EIGHT, usartDatabits9 = USART_FRAME_DATABITS_NINE, usartDatabits10 = USART_FRAME_DATABITS_TEN, usartDatabits11 = USART_FRAME_DATABITS_ELEVEN, usartDatabits12 = USART_FRAME_DATABITS_TWELVE, usartDatabits13 = USART_FRAME_DATABITS_THIRTEEN, usartDatabits14 = USART_FRAME_DATABITS_FOURTEEN, usartDatabits15 = USART_FRAME_DATABITS_FIFTEEN, usartDatabits16 = USART_FRAME_DATABITS_SIXTEEN } |
enum | USART_Enable_TypeDef { usartDisable = 0x0, usartEnableRx = USART_CMD_RXEN, usartEnableTx = USART_CMD_TXEN, usartEnable = (USART_CMD_RXEN | USART_CMD_TXEN) } |
enum | USART_HwFlowControl_TypeDef { usartHwFlowControlNone = 0, usartHwFlowControlCts, usartHwFlowControlRts, usartHwFlowControlCtsAndRts } |
enum | USART_I2sFormat_TypeDef { usartI2sFormatW32D32 = USART_I2SCTRL_FORMAT_W32D32, usartI2sFormatW32D24M = USART_I2SCTRL_FORMAT_W32D24M, usartI2sFormatW32D24 = USART_I2SCTRL_FORMAT_W32D24, usartI2sFormatW32D16 = USART_I2SCTRL_FORMAT_W32D16, usartI2sFormatW32D8 = USART_I2SCTRL_FORMAT_W32D8, usartI2sFormatW16D16 = USART_I2SCTRL_FORMAT_W16D16, usartI2sFormatW16D8 = USART_I2SCTRL_FORMAT_W16D8, usartI2sFormatW8D8 = USART_I2SCTRL_FORMAT_W8D8 } |
enum | USART_I2sJustify_TypeDef { usartI2sJustifyLeft = USART_I2SCTRL_JUSTIFY_LEFT, usartI2sJustifyRight = USART_I2SCTRL_JUSTIFY_RIGHT } |
enum | USART_IrDAPw_Typedef { usartIrDAPwONE = USART_IRCTRL_IRPW_ONE, usartIrDAPwTWO = USART_IRCTRL_IRPW_TWO, usartIrDAPwTHREE = USART_IRCTRL_IRPW_THREE, usartIrDAPwFOUR = USART_IRCTRL_IRPW_FOUR } |
enum | USART_OVS_TypeDef { usartOVS16 = USART_CTRL_OVS_X16, usartOVS8 = USART_CTRL_OVS_X8, usartOVS6 = USART_CTRL_OVS_X6, usartOVS4 = USART_CTRL_OVS_X4 } |
enum | USART_Parity_TypeDef { usartNoParity = USART_FRAME_PARITY_NONE, usartEvenParity = USART_FRAME_PARITY_EVEN, usartOddParity = USART_FRAME_PARITY_ODD } |
enum | USART_Stopbits_TypeDef { usartStopbits0p5 = USART_FRAME_STOPBITS_HALF, usartStopbits1 = USART_FRAME_STOPBITS_ONE, usartStopbits1p5 = USART_FRAME_STOPBITS_ONEANDAHALF, usartStopbits2 = USART_FRAME_STOPBITS_TWO } |
Functions | |
static void | prsIrInput (USART_TypeDef *usart, USART_PRS_Channel_t ch) |
Configure a PRS channel as USART Ir input. | |
static void | prsRxInput (USART_TypeDef *usart, USART_PRS_Channel_t ch) |
Configure a PRS channel as USART Rx input. | |
static void | prsTriggerInput (USART_TypeDef *usart, USART_PRS_Channel_t ch) |
Configure a PRS channel as USART Trigger input. | |
void | USART_BaudrateAsyncSet (USART_TypeDef *usart, uint32_t refFreq, uint32_t baudrate, USART_OVS_TypeDef ovs) |
Configure USART/UART operating in asynchronous mode to use a given baudrate (or as close as possible to a specified baudrate). | |
uint32_t | USART_BaudrateCalc (uint32_t refFreq, uint32_t clkdiv, bool syncmode, USART_OVS_TypeDef ovs) |
Calculate baudrate for USART/UART given reference frequency, clock division, and oversampling rate (if async mode). | |
uint32_t | USART_BaudrateGet (USART_TypeDef *usart) |
Get the current baudrate for USART/UART. | |
void | USART_BaudrateSyncSet (USART_TypeDef *usart, uint32_t refFreq, uint32_t baudrate) |
Configure the USART operating in synchronous mode to use a given baudrate (or as close as possible to a specified baudrate). | |
void | USART_Enable (USART_TypeDef *usart, USART_Enable_TypeDef enable) |
Enable/disable USART/UART receiver and/or transmitter. | |
void | USART_InitAsync (USART_TypeDef *usart, const USART_InitAsync_TypeDef *init) |
Initialize USART/UART for normal asynchronous mode. | |
void | USART_InitI2s (USART_TypeDef *usart, USART_InitI2s_TypeDef *init) |
Initialize USART for I2S mode. | |
__STATIC_INLINE void | USART_InitIrDA (const USART_InitIrDA_TypeDef *init) |
Initialization DEFAULT_IRDA_USART for asynchronous IrDA mode. | |
void | USART_InitPrsTrigger (USART_TypeDef *usart, const USART_PrsTriggerInit_TypeDef *init) |
Initialize the automatic transmissions using PRS channel as a trigger. | |
void | USART_InitSync (USART_TypeDef *usart, const USART_InitSync_TypeDef *init) |
Initialize USART for synchronous mode. | |
__STATIC_INLINE void | USART_IntClear (USART_TypeDef *usart, uint32_t flags) |
Clear one or more pending USART interrupts. | |
__STATIC_INLINE void | USART_IntDisable (USART_TypeDef *usart, uint32_t flags) |
Disable one or more USART interrupts. | |
__STATIC_INLINE void | USART_IntEnable (USART_TypeDef *usart, uint32_t flags) |
Enable one or more USART interrupts. | |
__STATIC_INLINE uint32_t | USART_IntGet (USART_TypeDef *usart) |
Get pending USART interrupt flags. | |
__STATIC_INLINE uint32_t | USART_IntGetEnabled (USART_TypeDef *usart) |
Get enabled and pending USART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
__STATIC_INLINE void | USART_IntSet (USART_TypeDef *usart, uint32_t flags) |
Set one or more pending USART interrupts from SW. | |
void | USART_Reset (USART_TypeDef *usart) |
Reset USART/UART to the same state that it was in after a hardware reset. | |
uint8_t | USART_Rx (USART_TypeDef *usart) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame). | |
__STATIC_INLINE uint8_t | USART_RxDataGet (USART_TypeDef *usart) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame). | |
__STATIC_INLINE uint16_t | USART_RxDataXGet (USART_TypeDef *usart) |
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information. | |
uint16_t | USART_RxDouble (USART_TypeDef *usart) |
Receive two 4-8 bit frames or one 10-16 bit frame. | |
uint32_t | USART_RxDoubleExt (USART_TypeDef *usart) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information. | |
__STATIC_INLINE uint16_t | USART_RxDoubleGet (USART_TypeDef *usart) |
Receive two 4-8 bit frames, or one 10-16 bit frame. | |
__STATIC_INLINE uint32_t | USART_RxDoubleXGet (USART_TypeDef *usart) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information. | |
uint16_t | USART_RxExt (USART_TypeDef *usart) |
Receive one 4-9 bit frame (or part of 10-16 bit frame) with extended information. | |
uint8_t | USART_SpiTransfer (USART_TypeDef *usart, uint8_t data) |
Perform one 8 bit frame SPI transfer. | |
__STATIC_INLINE uint32_t | USART_StatusGet (USART_TypeDef *usart) |
Get USART STATUS register. | |
void | USART_Tx (USART_TypeDef *usart, uint8_t data) |
Transmit one 4-9 bit frame. | |
void | USART_TxDouble (USART_TypeDef *usart, uint16_t data) |
Transmit two 4-9 bit frames or one 10-16 bit frame. | |
void | USART_TxDoubleExt (USART_TypeDef *usart, uint32_t data) |
Transmit two 4-9 bit frames or one 10-16 bit frame with extended control. | |
void | USART_TxExt (USART_TypeDef *usart, uint16_t data) |
Transmit one 4-9 bit frame with extended control. | |
void | USARTn_InitIrDA (USART_TypeDef *usart, const USART_InitIrDA_TypeDef *init) |
Initialize USART for asynchronous IrDA mode. | |
Macro Definition Documentation
#define USART_INITASYNC_DEFAULT |
Default configuration for USART asynchronous initialization structure.
Definition at line 379
of file em_usart.h
.
Referenced by BSP_BccInit(), RETARGET_SerialInit(), and UARTDRV_InitUart().
#define USART_INITI2S_DEFAULT |
Default configuration for I2S mode initialization structure.
Definition at line 684
of file em_usart.h
.
Referenced by MIC_init().
#define USART_INITIRDA_DEFAULT |
Default configuration for IrDA mode initialization structure.
Definition at line 588
of file em_usart.h
.
#define USART_INITPRSTRIGGER_DEFAULT |
Default configuration for USART PRS triggering structure.
Definition at line 400
of file em_usart.h
.
#define USART_INITSYNC_DEFAULT |
Default configuration for USART sync initialization structure.
Definition at line 500
of file em_usart.h
.
Referenced by MICROSD_Init(), and SPIDRV_Init().
#define usartIrDAPrsCh0 0U |
Deprecated PRS channel selector value. New code should use an integer instead.
Definition at line 208
of file em_usart.h
.
Typedef Documentation
typedef uint8_t USART_PRS_Channel_t |
PRS Channel type
Definition at line 204
of file em_usart.h
.
Enumeration Type Documentation
Clock polarity/phase mode.
Definition at line 174
of file em_usart.h
.
Databit selection.
Definition at line 102
of file em_usart.h
.
enum USART_Enable_TypeDef |
I2S format selection.
Definition at line 258
of file em_usart.h
.
enum USART_IrDAPw_Typedef |
Pulse width selection for IrDA mode.
Definition at line 189
of file em_usart.h
.
enum USART_OVS_TypeDef |
enum USART_Parity_TypeDef |
Function Documentation
|
static |
Configure a PRS channel as USART Ir input.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] ch
PRS channel.
Definition at line 214
of file em_usart.c
.
Referenced by USARTn_InitIrDA().
|
static |
Configure a PRS channel as USART Rx input.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] ch
PRS channel.
Definition at line 183
of file em_usart.c
.
Referenced by USART_InitAsync(), and USART_InitSync().
|
static |
Configure a PRS channel as USART Trigger input.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] ch
PRS channel.
Definition at line 244
of file em_usart.c
.
Referenced by USART_InitPrsTrigger().
void USART_BaudrateAsyncSet | ( | USART_TypeDef * | usart, |
uint32_t | refFreq, |
||
uint32_t | baudrate, |
||
USART_OVS_TypeDef | ovs |
||
) |
Configure USART/UART operating in asynchronous mode to use a given baudrate (or as close as possible to a specified baudrate).
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] refFreq
USART/UART reference clock frequency in Hz. If set to 0, the currently configured reference clock is assumed. [in] baudrate
Baudrate to try to achieve for USART/UART. [in] ovs
Oversampling to be used. Normal is 16x oversampling but lower oversampling may be used to achieve higher rates or better baudrate accuracy in some cases. Notice that lower oversampling frequency makes the channel more vulnerable to bit faults during reception due to clock inaccuracies compared to the link partner.
Definition at line 289
of file em_usart.c
.
References CMU_ClockFreqGet(), cmuClock_PCLK, usartOVS16, usartOVS4, usartOVS6, and usartOVS8.
Referenced by USART_InitAsync().
uint32_t USART_BaudrateCalc | ( | uint32_t | refFreq, |
uint32_t | clkdiv, |
||
bool | syncmode, |
||
USART_OVS_TypeDef | ovs |
||
) |
Calculate baudrate for USART/UART given reference frequency, clock division, and oversampling rate (if async mode).
This function returns the baudrate that a USART/UART module will use if configured with the given frequency, clock divisor, and mode. Notice that this function will not use the hardware configuration. It can be used to determine if a given configuration is sufficiently accurate for the application.
- Parameters
-
[in] refFreq
USART/UART HF peripheral frequency used. [in] clkdiv
A clock division factor to be used. [in] syncmode
- True - synchronous mode operation.
- False - asynchronous mode operation.
[in] ovs
Oversampling used if in asynchronous mode. Not used if syncmode
is true.
- Returns
- Baudrate with given settings.
Definition at line 429
of file em_usart.c
.
References usartOVS16, usartOVS6, and usartOVS8.
Referenced by USART_BaudrateGet().
uint32_t USART_BaudrateGet | ( | USART_TypeDef * | usart | ) |
Get the current baudrate for USART/UART.
This function returns the actual baudrate (not considering oscillator inaccuracies) used by a USART/UART peripheral.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block.
- Returns
- The current baudrate.
Definition at line 560
of file em_usart.c
.
References CMU_ClockFreqGet(), cmuClock_PCLK, and USART_BaudrateCalc().
Referenced by SPIDRV_GetBitrate().
void USART_BaudrateSyncSet | ( | USART_TypeDef * | usart, |
uint32_t | refFreq, |
||
uint32_t | baudrate |
||
) |
Configure the USART operating in synchronous mode to use a given baudrate (or as close as possible to a specified baudrate).
The configuration will be set to use a baudrate <= the specified baudrate to ensure that the baudrate does not exceed the specified value.
The fractional clock division is suppressed, although the hardware design allows it. It could cause half clock cycles to exceed a specified limit and thus potentially violate specifications for the slave device. In some special situations, a fractional clock division may be useful even in synchronous mode, but in those cases it must be directly adjusted, possibly assisted by USART_BaudrateCalc():
- Parameters
-
[in] usart
A pointer to the USART peripheral register block. (Cannot be used on UART modules.) [in] refFreq
A USART reference clock frequency in Hz that will be used. If set to 0, the currently-configured reference clock is assumed. [in] baudrate
Baudrate to try to achieve for USART.
Definition at line 617
of file em_usart.c
.
References CMU_ClockFreqGet(), and cmuClock_PCLK.
Referenced by MICROSD_SpiClkFast(), MICROSD_SpiClkSlow(), SPIDRV_SetBitrate(), and USART_InitSync().
void USART_Enable | ( | USART_TypeDef * | usart, |
USART_Enable_TypeDef | enable |
||
) |
Enable/disable USART/UART receiver and/or transmitter.
Notice that this function does not do any configuration. Enabling should normally be done after initialization (if not enabled as part of initialization).
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] enable
Select the status for the receiver/transmitter.
Definition at line 671
of file em_usart.c
.
References usartDisable.
Referenced by RETARGET_SerialInit(), UARTDRV_InitUart(), and USART_InitI2s().
void USART_InitAsync | ( | USART_TypeDef * | usart, |
const USART_InitAsync_TypeDef * | init |
||
) |
Initialize USART/UART for normal asynchronous mode.
This function will configure basic settings to operate in normal asynchronous mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly for the USART/UART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] init
A pointer to the initialization structure used to configure the basic async setup.
Definition at line 722
of file em_usart.c
.
References USART_InitAsync_TypeDef::autoCsEnable, USART_InitAsync_TypeDef::autoCsHold, USART_InitAsync_TypeDef::autoCsSetup, USART_InitAsync_TypeDef::baudrate, USART_InitAsync_TypeDef::databits, USART_InitAsync_TypeDef::enable, USART_InitAsync_TypeDef::hwFlowControl, USART_InitAsync_TypeDef::mvdis, USART_InitAsync_TypeDef::oversampling, USART_InitAsync_TypeDef::parity, USART_InitAsync_TypeDef::prsRxCh, USART_InitAsync_TypeDef::prsRxEnable, prsRxInput(), USART_InitAsync_TypeDef::refFreq, USART_InitAsync_TypeDef::stopbits, USART_BaudrateAsyncSet(), and USART_Reset().
Referenced by BSP_BccInit(), RETARGET_SerialInit(), UARTDRV_InitUart(), and USARTn_InitIrDA().
void USART_InitI2s | ( | USART_TypeDef * | usart, |
USART_InitI2s_TypeDef * | init |
||
) |
Initialize USART for I2S mode.
This function will configure basic settings to operate in I2S mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL and I2SCTRL registers.
Notice that pins used by the USART module must be properly configured by the user explicitly for the USART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usart
A pointer to the USART peripheral register block. (UART does not support this mode.) [in] init
A pointer to the initialization structure used to configure the basic I2S setup.
- Note
- This function does not apply to all USART's. See the chip Reference Manual.
Definition at line 954
of file em_usart.c
.
References USART_InitI2s_TypeDef::delay, USART_InitI2s_TypeDef::dmaSplit, USART_InitSync_TypeDef::enable, USART_InitI2s_TypeDef::format, USART_InitI2s_TypeDef::justify, USART_InitI2s_TypeDef::mono, USART_InitI2s_TypeDef::sync, USART_Enable(), USART_InitSync(), and usartDisable.
Referenced by MIC_init().
__STATIC_INLINE void USART_InitIrDA | ( | const USART_InitIrDA_TypeDef * | init | ) |
Initialization DEFAULT_IRDA_USART for asynchronous IrDA mode.
This function will configure basic settings in order to operate in asynchronous IrDA mode.
Special control setup not covered by this function must be done after using this function by direct modification of the CTRL and IRCTRL registers.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly for the USART/UART to work as intended. (When configuring pins, one should remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] init
Pointer to initialization structure used to configure asynchronous IrDA setup.
Deprecated:
- Deprecated function. New code should use USARTn_InitIrDA(). This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
Definition at line 765
of file em_usart.h
.
References USARTn_InitIrDA().
void USART_InitPrsTrigger | ( | USART_TypeDef * | usart, |
const USART_PrsTriggerInit_TypeDef * | init |
||
) |
Initialize the automatic transmissions using PRS channel as a trigger.
- Note
- Initialize USART with USART_Init() before setting up the PRS configuration.
- Parameters
-
[in] usart
A pointer to USART to configure. [in] init
A pointer to the initialization structure.
Definition at line 991
of file em_usart.c
.
References USART_PrsTriggerInit_TypeDef::autoTxTriggerEnable, USART_PrsTriggerInit_TypeDef::prsTriggerChannel, prsTriggerInput(), USART_PrsTriggerInit_TypeDef::rxTriggerEnable, and USART_PrsTriggerInit_TypeDef::txTriggerEnable.
void USART_InitSync | ( | USART_TypeDef * | usart, |
const USART_InitSync_TypeDef * | init |
||
) |
Initialize USART for synchronous mode.
This function will configure basic settings to operate in synchronous mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART module must be properly configured by the user explicitly for the USART to work as intended. (When configuring pins remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usart
A pointer to the USART peripheral register block. (UART does not support this mode.) [in] init
A pointer to the initialization structure used to configure basic async setup.
Definition at line 817
of file em_usart.c
.
References USART_InitSync_TypeDef::autoCsEnable, USART_InitSync_TypeDef::autoCsHold, USART_InitSync_TypeDef::autoCsSetup, USART_InitSync_TypeDef::autoTx, USART_InitSync_TypeDef::baudrate, USART_InitSync_TypeDef::clockMode, USART_InitSync_TypeDef::databits, USART_InitSync_TypeDef::enable, USART_InitSync_TypeDef::master, USART_InitSync_TypeDef::msbf, USART_InitSync_TypeDef::prsRxCh, USART_InitSync_TypeDef::prsRxEnable, prsRxInput(), USART_InitSync_TypeDef::refFreq, USART_BaudrateSyncSet(), and USART_Reset().
Referenced by ICM20648_spiInit(), MICROSD_Init(), SPI_TFT_Init(), SPIDRV_Init(), and USART_InitI2s().
__STATIC_INLINE void USART_IntClear | ( | USART_TypeDef * | usart, |
uint32_t | flags |
||
) |
Clear one or more pending USART interrupts.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block. [in] flags
Pending USART/UART interrupt source(s) to clear. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line 789
of file em_usart.h
.
Referenced by RETARGET_SerialInit(), and UARTDRV_InitUart().
__STATIC_INLINE void USART_IntDisable | ( | USART_TypeDef * | usart, |
uint32_t | flags |
||
) |
Disable one or more USART interrupts.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block. [in] flags
USART/UART interrupt source(s) to disable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line 809
of file em_usart.h
.
Referenced by disableRxInterrupt().
__STATIC_INLINE void USART_IntEnable | ( | USART_TypeDef * | usart, |
uint32_t | flags |
||
) |
Enable one or more USART interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using USART_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block. [in] flags
USART/UART interrupt source(s) to enable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line 830
of file em_usart.h
.
Referenced by enableRxInterrupt(), and RETARGET_SerialInit().
__STATIC_INLINE uint32_t USART_IntGet | ( | USART_TypeDef * | usart | ) |
Get pending USART interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- USART/UART interrupt source(s) pending. Returns one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line 849
of file em_usart.h
.
__STATIC_INLINE uint32_t USART_IntGetEnabled | ( | USART_TypeDef * | usart | ) |
Get enabled and pending USART interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- Pending and enabled USART interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in USARTx_IEN_nnn register (USARTx_IEN_nnn) and
- the OR combination of valid interrupt flags of the USART module (USARTx_IF_nnn).
Definition at line 873
of file em_usart.h
.
__STATIC_INLINE void USART_IntSet | ( | USART_TypeDef * | usart, |
uint32_t | flags |
||
) |
Set one or more pending USART interrupts from SW.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block. [in] flags
USART/UART interrupt source(s) to set to pending. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
Definition at line 896
of file em_usart.h
.
void USART_Reset | ( | USART_TypeDef * | usart | ) |
Reset USART/UART to the same state that it was in after a hardware reset.
- Parameters
-
[in] usart
A pointer to USART/UART peripheral register block.
Definition at line 1025
of file em_usart.c
.
Referenced by BOARD_flashDeepPowerDown(), BSP_BccDeInit(), ICM20648_spiInit(), MIC_deInit(), MICROSD_Deinit(), SPI_TFT_Init(), SPIDRV_DeInit(), USART_InitAsync(), and USART_InitSync().
uint8_t USART_Rx | ( | USART_TypeDef * | usart | ) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
This function is normally used to receive one frame when operating with frame length 4-8 bits. See USART_RxExt() for reception of 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call USART_RxDataGet() to read the RXDATA register directly.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1120
of file em_usart.c
.
Referenced by ICM20648_bankSelect(), ICM20648_registerRead(), ICM20648_registerWrite(), and SPI_TFT_WriteRegister().
__STATIC_INLINE uint8_t USART_RxDataGet | ( | USART_TypeDef * | usart | ) |
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
This function is used to quickly receive one 4-8 bits frame by reading the RXDATA register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data. Please refer to USART_RxDataXGet() for reception of 9 bit frames.
- Note
- Since this function does not check whether the RXDATA register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The USART_Rx() is normally a better choice if the validity of the RXDATA register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 955
of file em_usart.h
.
__STATIC_INLINE uint16_t USART_RxDataXGet | ( | USART_TypeDef * | usart | ) |
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
This function is used to quickly receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information by reading the RXDATAX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data.
- Note
- Since this function does not check whether the RXDATAX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The USART_RxExt() is normally a better choice if the validity of the RXDATAX register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1061
of file em_usart.h
.
uint16_t USART_RxDouble | ( | USART_TypeDef * | usart | ) |
Receive two 4-8 bit frames or one 10-16 bit frame.
This function is normally used to receive one frame when operating with frame length 10-16 bits. See USART_RxDoubleExt() for reception of two 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call USART_RxDoubleGet() to read the RXDOUBLE register directly.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1152
of file em_usart.c
.
uint32_t USART_RxDoubleExt | ( | USART_TypeDef * | usart | ) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
This function is normally used to receive one frame when operating with frame length 10-16 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call USART_RxDoubleXGet() to read the RXDOUBLEX register directly.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1184
of file em_usart.c
.
__STATIC_INLINE uint16_t USART_RxDoubleGet | ( | USART_TypeDef * | usart | ) |
Receive two 4-8 bit frames, or one 10-16 bit frame.
This function is used to quickly receive one 10-16 bits frame or two 4-8 bit frames by reading the RXDOUBLE register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data. This function is normally used to receive one frame when operating with frame length 10-16 bits. Please refer to USART_RxDoubleXGet() for reception of two 9 bit frames.
- Note
- Since this function does not check whether the RXDOUBLE register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The USART_RxDouble() is normally a better choice if the validity of the RXDOUBLE register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 992
of file em_usart.h
.
__STATIC_INLINE uint32_t USART_RxDoubleXGet | ( | USART_TypeDef * | usart | ) |
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
This function is used to quickly receive one 10-16 bits frame or two 4-9 bit frames by reading the RXDOUBLEX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data.
- Note
- Since this function does not check whether the RXDOUBLEX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The USART_RxDoubleExt() is normally a better choice if the validity of the RXDOUBLEX register is not certain.
- Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1027
of file em_usart.h
.
uint16_t USART_RxExt | ( | USART_TypeDef * | usart | ) |
Receive one 4-9 bit frame (or part of 10-16 bit frame) with extended information.
This function is normally used to receive one frame when operating with frame length 4-9 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call USART_RxDataXGet() to read the RXDATAX register directly.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block.
- Returns
- Data received.
Definition at line 1216
of file em_usart.c
.
uint8_t USART_SpiTransfer | ( | USART_TypeDef * | usart, |
uint8_t | data |
||
) |
Perform one 8 bit frame SPI transfer.
- Note
- This function will stall if the transmit buffer is full. When a transmit buffer becomes available, data is written and the function will wait until data is fully transmitted. The SPI return value is then read out and returned.
- Parameters
-
[in] usart
A pointer to the USART peripheral register block. [in] data
Data to transmit.
- Returns
- Data received.
Definition at line 1243
of file em_usart.c
.
Referenced by BOARD_flashDeepPowerDown(), and MICROSD_XferSpi().
__STATIC_INLINE uint32_t USART_StatusGet | ( | USART_TypeDef * | usart | ) |
Get USART STATUS register.
- Parameters
-
[in] usart
Pointer to USART/UART peripheral register block.
- Returns
- STATUS register value.
Definition at line 916
of file em_usart.h
.
void USART_Tx | ( | USART_TypeDef * | usart, |
uint8_t | data |
||
) |
Transmit one 4-9 bit frame.
Depending on the frame length configuration, 4-8 (least significant) bits from data
are transmitted. If the frame length is 9, 8 bits are transmitted from data
and one bit as specified by CTRL register, BIT8DV field. See USART_TxExt() for transmitting 9 bit frame with full control of all 9 bits.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is full until the buffer becomes available.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] data
Data to transmit. See details above for more information.
Definition at line 1276
of file em_usart.c
.
Referenced by ICM20648_bankSelect(), ICM20648_registerRead(), ICM20648_registerWrite(), SPI_TFT_WriteRegister(), and UARTDRV_ForceTransmit().
void USART_TxDouble | ( | USART_TypeDef * | usart, |
uint16_t | data |
||
) |
Transmit two 4-9 bit frames or one 10-16 bit frame.
Depending on the frame length configuration, 4-8 (least significant) bits from each byte in data
are transmitted. If frame length is 9, 8 bits are transmitted from each byte in data
adding one bit as specified by the CTRL register, BIT8DV field, to each byte. See USART_TxDoubleExt() for transmitting two 9 bit frames with full control of all 9 bits.
If the frame length is 10-16, 10-16 (least significant) bits from data
are transmitted.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is full until the buffer becomes available.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] data
Data to transmit, the least significant byte holds the frame transmitted first. See details above for more info.
Definition at line 1311
of file em_usart.c
.
void USART_TxDoubleExt | ( | USART_TypeDef * | usart, |
uint32_t | data |
||
) |
Transmit two 4-9 bit frames or one 10-16 bit frame with extended control.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is full until the buffer becomes available.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] data
Data to transmit with extended control. Contains two 16 bit words concatenated. Least significant word holds the frame transmitted first. If the frame length is 4-9, two frames with 4-9 least significant bits from each 16 bit word are transmitted.
- If the frame length is 10-16 bits, 8 data bits are taken from the least significant 16 bit word and the remaining bits from the other 16 bit word.
- Additional control bits are available as documented in the reference manual (set to 0 if not used). For 10-16 bit frame length, these control bits are taken from the most significant 16 bit word.
Definition at line 1346
of file em_usart.c
.
void USART_TxExt | ( | USART_TypeDef * | usart, |
uint16_t | data |
||
) |
Transmit one 4-9 bit frame with extended control.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
- Note
- This function will stall if the buffer is full until the buffer becomes available.
- Parameters
-
[in] usart
A pointer to the USART/UART peripheral register block. [in] data
Data to transmit with extended control. Least significant bit contains frame bits. Additional control bits are available as documented in the reference manual (set to 0 if not used).
Definition at line 1373
of file em_usart.c
.
void USARTn_InitIrDA | ( | USART_TypeDef * | usart, |
const USART_InitIrDA_TypeDef * | init |
||
) |
Initialize USART for asynchronous IrDA mode.
This function will configure basic settings to operate in asynchronous IrDA mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL and IRCTRL registers.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly for the USART/UART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
- Parameters
-
[in] usart
A pointer to the USART peripheral register block. [in] init
A pointer to the initialization structure used to configure async IrDA setup.
- Note
- Not all USART instances support IrDA. See the data sheet for your device.
Definition at line 898
of file em_usart.c
.
References USART_InitIrDA_TypeDef::async, USART_InitIrDA_TypeDef::irFilt, USART_InitIrDA_TypeDef::irPrsEn, USART_InitIrDA_TypeDef::irPrsSel, USART_InitIrDA_TypeDef::irPw, USART_InitIrDA_TypeDef::irRxInv, prsIrInput(), and USART_InitAsync().
Referenced by USART_InitIrDA().