Definition at line 351
of file em_se.h
.
Data Fields | |
bool | enableAntiRollback |
bool | enableSecureBoot |
bool | secureBootPageLockFull |
bool | secureBootPageLockNarrow |
bool | verifySecureBootCertificate |
Field Documentation
bool SE_OTPInit_t::enableAntiRollback |
Enable anti-rollback for host application upgrades.
Definition at line 357
of file em_se.h
.
Referenced by SE_initOTP().
bool SE_OTPInit_t::enableSecureBoot |
Enable secure boot for the host.
Definition at line 353
of file em_se.h
.
Referenced by SE_initOTP().
bool SE_OTPInit_t::secureBootPageLockFull |
Set flag to enable locking down all flash pages that cover the secure-booted image, including the last page if end of signature is not page-aligned.
Definition at line 366
of file em_se.h
.
Referenced by SE_initOTP().
bool SE_OTPInit_t::secureBootPageLockNarrow |
Set flag to enable locking down all flash pages that cover the secure-booted image, except the last page if end of signature is not page-aligned.
Definition at line 362
of file em_se.h
.
Referenced by SE_initOTP().
bool SE_OTPInit_t::verifySecureBootCertificate |
Require certificate based secure boot signing.
Definition at line 355
of file em_se.h
.
Referenced by SE_initOTP().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_se.h