SE_Command_t Struct Reference

SE Command structure to which all commands to the SE must adhere.

Definition at line 330 of file em_se.h .

#include < em_se.h >

Data Fields

uint32_t command
SE_DataTransfer_t * data_in
SE_DataTransfer_t * data_out
size_t num_parameters
uint32_t parameters [ SE_MAX_PARAMETERS ]

The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_se.h