BURTC_Init_TypeDef Struct Reference

BURTC initialization structure for Series 2 devices.

Definition at line 145 of file em_burtc.h .

#include < em_burtc.h >

Data Fields

uint32_t clkDiv
bool compare0Top
bool debugRun
bool em4comp
bool em4overflow
bool start

Field Documentation

uint32_t BURTC_Init_TypeDef::clkDiv

Clock divider. Supported range is 1-32768

Definition at line 148 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::compare0Top

Set if Compare Value 0 is also top value (counter restart)

Definition at line 149 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::debugRun

If true, counter will keep running under debug halt

Definition at line 147 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::em4comp

Enable EM4 wakeup on compare match.

Definition at line 150 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::em4overflow

Enable EM4 wakeup on counter overflow.

Definition at line 151 of file em_burtc.h .

Referenced by BURTC_Init() .

bool BURTC_Init_TypeDef::start

Start BURTC after initialization

Definition at line 146 of file em_burtc.h .

Referenced by BURTC_Init() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/ em_burtc.h