Border Agent#

This module includes functions for the Thread Border Agent role.

Enumerations#

enum
OT_BORDER_AGENT_STATE_STOPPED = 0
OT_BORDER_AGENT_STATE_STARTED = 1
OT_BORDER_AGENT_STATE_ACTIVE = 2
}

This enumeration defines the Border Agent state.

Typedefs#

typedef enum otBorderAgentState

This enumeration defines the Border Agent state.

Functions#

otBorderAgentGetState(otInstance *aInstance)

Gets the otBorderAgentState of the Thread Border Agent role.

uint16_t
otBorderAgentGetUdpPort(otInstance *aInstance)

Gets the UDP port of the Thread Border Agent service.

otBorderAgentGetId(otInstance *aInstance, uint8_t *aId, uint16_t *aLength)

Gets the randomly generated Border Agent ID.

Macros#

#define

The length of Border Agent/Router ID in bytes.

Enumeration Documentation#

otBorderAgentState#

otBorderAgentState

This enumeration defines the Border Agent state.

Enumerator
OT_BORDER_AGENT_STATE_STOPPED

Border agent role is disabled.

OT_BORDER_AGENT_STATE_STARTED

Border agent is started.

OT_BORDER_AGENT_STATE_ACTIVE

Border agent is connected with external commissioner.


Typedef Documentation#

otBorderAgentState#

typedef enum otBorderAgentState otBorderAgentState

This enumeration defines the Border Agent state.


Function Documentation#

otBorderAgentGetState#

otBorderAgentState otBorderAgentGetState (otInstance * aInstance)

Gets the otBorderAgentState of the Thread Border Agent role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns


otBorderAgentGetUdpPort#

uint16_t otBorderAgentGetUdpPort (otInstance * aInstance)

Gets the UDP port of the Thread Border Agent service.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • UDP port of the Border Agent.


otBorderAgentGetId#

otError otBorderAgentGetId (otInstance * aInstance, uint8_t * aId, uint16_t * aLength)

Gets the randomly generated Border Agent ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[out]aId

A pointer to buffer to receive the ID.

uint16_t *[inout]aLength

Specifies the length of aId when used as input and receives the length actual ID data copied to aId when used as output.

The ID is saved in persistent storage and survives reboots. The typical use case of the ID is to be published in the MeshCoP mDNS service as the id TXT value for the client to identify this Border Router/Agent device.


Macro Definition Documentation#

OT_BORDER_AGENT_ID_LENGTH#

#define OT_BORDER_AGENT_ID_LENGTH
Value:
(16)

The length of Border Agent/Router ID in bytes.