This type represents information about a router in Thread mesh.
Public Attributes#
Extended MAC address.
RLOC16.
Router ID.
Thread Version. OT_MESH_DIAG_VERSION_UNKNOWN if unknown.
Whether router is this device itself.
Whether router is parent of this device (when device is a child).
Whether router is leader.
Whether router acts as a border router providing ext connectivity.
This array provides the link quality from this router to other routers, also indicating whether a link is established between the routers.
A pointer to an iterator to go through the list of IPv6 addresses of the router.
A pointer to an iterator to go through the list of children of the router.
Public Attribute Documentation#
mVersion#
uint16_t otMeshDiagRouterInfo::mVersion
Thread Version. OT_MESH_DIAG_VERSION_UNKNOWN if unknown.
mIsThisDeviceParent#
bool otMeshDiagRouterInfo::mIsThisDeviceParent
Whether router is parent of this device (when device is a child).
mIsBorderRouter#
bool otMeshDiagRouterInfo::mIsBorderRouter
Whether router acts as a border router providing ext connectivity.
mLinkQualities#
uint8_t otMeshDiagRouterInfo::mLinkQualities[OT_NETWORK_MAX_ROUTER_ID+1]
This array provides the link quality from this router to other routers, also indicating whether a link is established between the routers.
The array is indexed based on Router ID. mLinkQualities[routerId] indicates the incoming link quality, the router sees to the router with routerId. Link quality is a value in [0, 3]. Value zero indicates no link. Larger value indicate better link quality (as defined by Thread specification).
mIp6AddrIterator#
otMeshDiagIp6AddrIterator* otMeshDiagRouterInfo::mIp6AddrIterator
A pointer to an iterator to go through the list of IPv6 addresses of the router.
The pointer is valid only while otMeshDiagRouterInfo is valid. It can be used in otMeshDiagGetNextIp6Address to iterate through the IPv6 addresses.
The pointer can be NULL when there was no request to discover IPv6 addresses (in otMeshDiagDiscoverConfig) or if the router did not provide the list.
mChildIterator#
otMeshDiagChildIterator* otMeshDiagRouterInfo::mChildIterator
A pointer to an iterator to go through the list of children of the router.
The pointer is valid only while otMeshDiagRouterInfo is valid. It can be used in otMeshDiagGetNextChildInfo to iterate through the children of the router.
The pointer can be NULL when there was no request to discover children (in otMeshDiagDiscoverConfig) or if the router did not provide the list.