Server#
This module includes functions to manage local network data with the OpenThread Server.
Functions#
Provides a full or stable copy of the local Thread Network Data.
Add a service configuration to the local network data.
Remove a service configuration from the local network data.
Gets the next service in the local Network Data.
Immediately register the local network data with the Leader.
Function Documentation#
otServerGetNetDataLocal#
otError otServerGetNetDataLocal (otInstance * aInstance, bool aStable, uint8_t * aData, uint8_t * aDataLength)
Provides a full or stable copy of the local Thread Network Data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| bool | [in] | aStable | TRUE when copying the stable version, FALSE when copying the full version. |
| uint8_t * | [out] | aData | A pointer to the data buffer. |
| uint8_t * | [inout] | aDataLength | On entry, size of the data buffer pointed to by |
otServerAddService#
otError otServerAddService (otInstance * aInstance, const otServiceConfig * aConfig)
Add a service configuration to the local network data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| const otServiceConfig * | [in] | aConfig | A pointer to the service configuration. |
See Also
otServerRemoveService#
otError otServerRemoveService (otInstance * aInstance, uint32_t aEnterpriseNumber, const uint8_t * aServiceData, uint8_t aServiceDataLength)
Remove a service configuration from the local network data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| uint32_t | [in] | aEnterpriseNumber | Enterprise Number of the service entry to be deleted. |
| const uint8_t * | [in] | aServiceData | A pointer to an Service Data to look for during deletion. |
| uint8_t | [in] | aServiceDataLength | The length of |
See Also
otServerGetNextService#
otError otServerGetNextService (otInstance * aInstance, otNetworkDataIterator * aIterator, otServiceConfig * aConfig)
Gets the next service in the local Network Data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otNetworkDataIterator * | [inout] | aIterator | A pointer to the Network Data iterator context. To get the first service entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| otServiceConfig * | [out] | aConfig | A pointer to where the service information will be placed. |
otServerRegister#
otError otServerRegister (otInstance * aInstance)
Immediately register the local network data with the Leader.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
See Also