Represents a Commissioning Dataset.

Public Attributes#

uint16_t

Border Router RLOC16.

uint16_t

Commissioner Session Id.

uint16_t

Joiner UDP Port.

bool

TRUE if Border Router RLOC16 is set, FALSE otherwise.

bool

TRUE if Commissioner Session Id is set, FALSE otherwise.

bool

TRUE if Steering Data is set, FALSE otherwise.

bool

TRUE if Joiner UDP Port is set, FALSE otherwise.

Public Attribute Documentation#

mLocator#

uint16_t otCommissioningDataset::mLocator

Border Router RLOC16.


mSessionId#

uint16_t otCommissioningDataset::mSessionId

Commissioner Session Id.


mSteeringData#

otSteeringData otCommissioningDataset::mSteeringData

Steering Data.


mJoinerUdpPort#

uint16_t otCommissioningDataset::mJoinerUdpPort

Joiner UDP Port.


mIsLocatorSet#

bool otCommissioningDataset::mIsLocatorSet

TRUE if Border Router RLOC16 is set, FALSE otherwise.


mIsSessionIdSet#

bool otCommissioningDataset::mIsSessionIdSet

TRUE if Commissioner Session Id is set, FALSE otherwise.


mIsSteeringDataSet#

bool otCommissioningDataset::mIsSteeringDataSet

TRUE if Steering Data is set, FALSE otherwise.


mIsJoinerUdpPortSet#

bool otCommissioningDataset::mIsJoinerUdpPortSet

TRUE if Joiner UDP Port is set, FALSE otherwise.