Channel Manager#
This module includes functions for Channel Manager.
The functions in this module are available when Channel Manager features OPENTHREAD_CONFIG_CHANNEL_MANAGER_ENABLE or OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE are enabled. Channel Manager behavior depends on the device role. It manages the network-wide PAN channel on a Full Thread Device in rx-on-when-idle mode, or with OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE set, selects CSL channel in synchronized rx-off-when-idle mode. On a Minimal Thread Device OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE selects the CSL channel. 
Functions#
Requests a Thread network channel change.
Gets the channel from the last successful call to otChannelManagerRequestChannelChange()
Gets the delay (in seconds) used by Channel Manager for a network channel change.
Sets the delay (in seconds) used for a network channel change.
Requests that ChannelManager checks and selects a new channel and starts a channel change. 
Requests that ChannelManager checks and selects a new CSL channel and starts a CSL channel change. 
Enables or disables the auto-channel-selection functionality for network channel.
Indicates whether the auto-channel-selection functionality for a network channel is enabled or not.
Enables or disables the auto-channel-selection functionality for a CSL channel.
Indicates whether the auto-csl-channel-selection functionality is enabled or not.
Sets the period interval (in seconds) used by auto-channel-selection functionality.
Gets the period interval (in seconds) used by auto-channel-selection functionality.
Gets the supported channel mask.
Sets the supported channel mask.
Gets the favored channel mask.
Sets the favored channel mask.
Gets the CCA failure rate threshold.
Sets the CCA failure rate threshold.
Function Documentation#
otChannelManagerRequestChannelChange#
void otChannelManagerRequestChannelChange (otInstance * aInstance, uint8_t aChannel)
Requests a Thread network channel change.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint8_t | [in] | aChannel | The new channel for the Thread network. | 
The network switches to the given channel after a specified delay (see otChannelManagerSetDelay()). The channel change is performed by updating the Pending Operational Dataset.
A subsequent call will cancel an ongoing previously requested channel change.
otChannelManagerGetRequestedChannel#
uint8_t otChannelManagerGetRequestedChannel (otInstance * aInstance)
Gets the channel from the last successful call to otChannelManagerRequestChannelChange()
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | N/A | aInstance | 
Returns
- The last requested channel or zero if there has been no channel change request yet. 
otChannelManagerGetDelay#
uint16_t otChannelManagerGetDelay (otInstance * aInstance)
Gets the delay (in seconds) used by Channel Manager for a network channel change.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Only available on FTDs.
Returns
- The delay (in seconds) for channel change. 
otChannelManagerSetDelay#
otError otChannelManagerSetDelay (otInstance * aInstance, uint16_t aDelay)
Sets the delay (in seconds) used for a network channel change.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint16_t | [in] | aDelay | Delay in seconds. | 
Only available on FTDs. The delay should preferably be longer than the maximum data poll interval used by all Sleepy End Devices within the Thread network.
otChannelManagerRequestChannelSelect#
otError otChannelManagerRequestChannelSelect (otInstance * aInstance, bool aSkipQualityCheck)
Requests that ChannelManager checks and selects a new channel and starts a channel change. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| bool | [in] | aSkipQualityCheck | Indicates whether the quality check (step 1) should be skipped. | 
Unlike the otChannelManagerRequestChannelChange() where the channel must be given as a parameter, this function asks the ChannelManager to select a channel by itself (based on collected channel quality info).
Once called, the Channel Manager will perform the following 3 steps:
1) ChannelManager decides if the channel change would be helpful. This check can be skipped if aSkipQualityCheck is set to true (forcing a channel selection to happen and skipping the quality check). This step uses the collected link quality metrics on the device (such as CCA failure rate, frame and message error rates per neighbor, etc.) to determine if the current channel quality is at the level that justifies a channel change.
2) If the first step passes, then ChannelManager selects a potentially better channel. It uses the collected channel quality data by ChannelMonitor module. The supported and favored channels are used at this step. (see otChannelManagerSetSupportedChannels() and otChannelManagerSetFavoredChannels()).
3) If the newly selected channel is different from the current channel, ChannelManager requests/starts the channel change process (internally invoking a RequestChannelChange()).
otChannelManagerRequestCslChannelSelect#
otError otChannelManagerRequestCslChannelSelect (otInstance * aInstance, bool aSkipQualityCheck)
Requests that ChannelManager checks and selects a new CSL channel and starts a CSL channel change. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| bool | [in] | aSkipQualityCheck | Indicates whether the quality check (step 1) should be skipped. | 
Only available with OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE. This function asks the ChannelManager to select a channel by itself (based on collected channel quality info).
Once called, the Channel Manager will perform the following 3 steps:
1) ChannelManager decides if the CSL channel change would be helpful. This check can be skipped if aSkipQualityCheck is set to true (forcing a CSL channel selection to happen and skipping the quality check). This step uses the collected link quality metrics on the device (such as CCA failure rate, frame and message error rates per neighbor, etc.) to determine if the current channel quality is at the level that justifies a CSL channel change.
2) If the first step passes, then ChannelManager selects a potentially better CSL channel. It uses the collected channel quality data by ChannelMonitor module. The supported and favored channels are used at this step. (see otChannelManagerSetSupportedChannels() and otChannelManagerSetFavoredChannels()).
3) If the newly selected CSL channel is different from the current CSL channel, ChannelManager starts the CSL channel change process.
otChannelManagerSetAutoChannelSelectionEnabled#
void otChannelManagerSetAutoChannelSelectionEnabled (otInstance * aInstance, bool aEnabled)
Enables or disables the auto-channel-selection functionality for network channel.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| bool | [in] | aEnabled | Indicates whether to enable or disable this functionality. | 
When enabled, ChannelManager will periodically invoke a RequestChannelSelect(false). The period interval can be set by otChannelManagerSetAutoChannelSelectionInterval().
otChannelManagerGetAutoChannelSelectionEnabled#
bool otChannelManagerGetAutoChannelSelectionEnabled (otInstance * aInstance)
Indicates whether the auto-channel-selection functionality for a network channel is enabled or not.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- TRUE if enabled, FALSE if disabled. 
otChannelManagerSetAutoCslChannelSelectionEnabled#
void otChannelManagerSetAutoCslChannelSelectionEnabled (otInstance * aInstance, bool aEnabled)
Enables or disables the auto-channel-selection functionality for a CSL channel.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| bool | [in] | aEnabled | Indicates whether to enable or disable this functionality. | 
Only available with OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE. When enabled, ChannelManager will periodically invoke a otChannelManagerRequestCslChannelSelect(). The period interval can be set by otChannelManagerSetAutoChannelSelectionInterval().
otChannelManagerGetAutoCslChannelSelectionEnabled#
bool otChannelManagerGetAutoCslChannelSelectionEnabled (otInstance * aInstance)
Indicates whether the auto-csl-channel-selection functionality is enabled or not.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Only available with OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE && OPENTHREAD_CONFIG_CHANNEL_MANAGER_CSL_CHANNEL_SELECT_ENABLE.
Returns
- TRUE if enabled, FALSE if disabled. 
otChannelManagerSetAutoChannelSelectionInterval#
otError otChannelManagerSetAutoChannelSelectionInterval (otInstance * aInstance, uint32_t aInterval)
Sets the period interval (in seconds) used by auto-channel-selection functionality.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint32_t | [in] | aInterval | The interval in seconds. | 
otChannelManagerGetAutoChannelSelectionInterval#
uint32_t otChannelManagerGetAutoChannelSelectionInterval (otInstance * aInstance)
Gets the period interval (in seconds) used by auto-channel-selection functionality.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- The interval in seconds. 
otChannelManagerGetSupportedChannels#
uint32_t otChannelManagerGetSupportedChannels (otInstance * aInstance)
Gets the supported channel mask.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- The supported channels as a bit-mask. 
otChannelManagerSetSupportedChannels#
void otChannelManagerSetSupportedChannels (otInstance * aInstance, uint32_t aChannelMask)
Sets the supported channel mask.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint32_t | [in] | aChannelMask | A channel mask. | 
otChannelManagerGetFavoredChannels#
uint32_t otChannelManagerGetFavoredChannels (otInstance * aInstance)
Gets the favored channel mask.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- The favored channels as a bit-mask. 
otChannelManagerSetFavoredChannels#
void otChannelManagerSetFavoredChannels (otInstance * aInstance, uint32_t aChannelMask)
Sets the favored channel mask.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint32_t | [in] | aChannelMask | A channel mask. | 
otChannelManagerGetCcaFailureRateThreshold#
uint16_t otChannelManagerGetCcaFailureRateThreshold (otInstance * aInstance)
Gets the CCA failure rate threshold.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- The CCA failure rate threshold. Value 0 maps to 0% and 0xffff maps to 100%. 
otChannelManagerSetCcaFailureRateThreshold#
void otChannelManagerSetCcaFailureRateThreshold (otInstance * aInstance, uint16_t aThreshold)
Sets the CCA failure rate threshold.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| uint16_t | [in] | aThreshold | A CCA failure rate threshold. Value 0 maps to 0% and 0xffff maps to 100%. |