Heap#
This module includes functions that set the external OpenThread heap.
Function Documentation#
otHeapCAlloc#
void * otHeapCAlloc (size_t aCount, size_t aSize)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| size_t | N/A | aCount | |
| size_t | N/A | aSize | 
Note
- This API is deprecated and use of it is discouraged. 
otHeapFree#
void otHeapFree (void * aPointer)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void * | N/A | aPointer | 
Note
- This API is deprecated and use of it is discouraged.