Network Time Synchronization#
This module includes functions that control network time synchronization service.
Enumerations#
Represents OpenThread time synchronization status.
Typedefs#
Represents OpenThread time synchronization status.
Pointer is called when a network time sync or status change occurs.
Functions#
Get the Thread network time.
Set the time synchronization period.
Get the time synchronization period.
Set the time synchronization XTAL accuracy threshold for Router-Capable device.
Get the time synchronization XTAL accuracy threshold for Router.
Set a callback to be called when a network time sync or status change occurs.
Macros#
zero is considered as invalid time synchronization sequence.
Enumeration Documentation#
otNetworkTimeStatus#
otNetworkTimeStatus
Represents OpenThread time synchronization status.
| Enumerator | |
|---|---|
| OT_NETWORK_TIME_UNSYNCHRONIZED | The device hasn't attached to a network. | 
| OT_NETWORK_TIME_RESYNC_NEEDED | The device hasn’t received time sync for more than two periods time. | 
| OT_NETWORK_TIME_SYNCHRONIZED | The device network time is synchronized. | 
Typedef Documentation#
otNetworkTimeStatus#
typedef enum otNetworkTimeStatus otNetworkTimeStatus
Represents OpenThread time synchronization status.
otNetworkTimeSyncCallbackFn#
typedef void(* otNetworkTimeSyncCallbackFn) (void *aCallbackContext) )(void *aCallbackContext)
Pointer is called when a network time sync or status change occurs.
Function Documentation#
otNetworkTimeGet#
otNetworkTimeStatus otNetworkTimeGet (otInstance * aInstance, uint64_t * aNetworkTime)
Get the Thread network time.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| uint64_t * | [inout] | aNetworkTime | The Thread network time in microseconds. | 
Returns
- The time synchronization status. 
otNetworkTimeSetSyncPeriod#
otError otNetworkTimeSetSyncPeriod (otInstance * aInstance, uint16_t aTimeSyncPeriod)
Set the time synchronization period.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| uint16_t | [in] | aTimeSyncPeriod | The time synchronization period, in seconds. | 
Can only be called while Thread protocols are disabled.
otNetworkTimeGetSyncPeriod#
uint16_t otNetworkTimeGetSyncPeriod (otInstance * aInstance)
Get the time synchronization period.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
Returns
- The time synchronization period. 
otNetworkTimeSetXtalThreshold#
otError otNetworkTimeSetXtalThreshold (otInstance * aInstance, uint16_t aXTALThreshold)
Set the time synchronization XTAL accuracy threshold for Router-Capable device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| uint16_t | [in] | aXTALThreshold | The XTAL accuracy threshold for Router, in PPM. | 
Can only be called while Thread protocols are disabled.
otNetworkTimeGetXtalThreshold#
uint16_t otNetworkTimeGetXtalThreshold (otInstance * aInstance)
Get the time synchronization XTAL accuracy threshold for Router.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
Returns
- The XTAL accuracy threshold for Router, in PPM. 
otNetworkTimeSyncSetCallback#
void otNetworkTimeSyncSetCallback (otInstance * aInstance, otNetworkTimeSyncCallbackFn aCallbackFn, void * aCallbackContext)
Set a callback to be called when a network time sync or status change occurs.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| otNetworkTimeSyncCallbackFn | [in] | aCallbackFn | The callback function to be called | 
| void * | [in] | aCallbackContext | The context to be passed to the callback function upon invocation | 
This callback shall be called only when the network time offset jumps by OPENTHREAD_CONFIG_TIME_SYNC_JUMP_NOTIF_MIN_US or when the status changes.