Mesh Diagnostics#
This module includes definitions and functions for Mesh Diagnostics.
The Mesh Diagnostics APIs require OPENTHREAD_CONFIG_MESH_DIAG_ENABLE and OPENTHREAD_FTD. 
Modules#
Typedefs#
Represents the set of configurations used when discovering mesh topology indicating which items to discover.
An opaque iterator to iterate over list of IPv6 addresses of a router.
An opaque iterator to iterate over list of children of a router.
Represents information about a router in Thread mesh discovered using otMeshDiagDiscoverTopology(). 
Represents information about a discovered child in Thread mesh using otMeshDiagDiscoverTopology(). 
Pointer type represents the callback used by otMeshDiagDiscoverTopology() to provide information about a discovered router. 
Represents information about a child entry from otMeshDiagQueryChildTable(). 
Represents the callback used by otMeshDiagQueryChildTable() to provide information about child table entries. 
Represents the callback used by otMeshDiagQueryChildrenIp6Addrs() to provide information about an MTD child and its list of IPv6 addresses. 
Represents information about a router neighbor entry from otMeshDiagQueryRouterNeighborTable(). 
Represents the callback used by otMeshDiagQueryRouterNeighborTable() to provide information about neighbor router table entries. 
Functions#
Starts network topology discovery.
Cancels an ongoing topology discovery if there is one, otherwise no action.
Iterates through the discovered IPv6 addresses of a router or an MTD child.
Iterates through the discovered children of a router.
Starts query for child table for a given router.
Sends a query to a parent to retrieve the IPv6 addresses of all its MTD children.
Starts query for router neighbor table for a given router.
Macros#
Specifies that Thread Version is unknown.
Typedef Documentation#
otMeshDiagDiscoverConfig#
typedef struct otMeshDiagDiscoverConfig otMeshDiagDiscoverConfig
Represents the set of configurations used when discovering mesh topology indicating which items to discover.
otMeshDiagIp6AddrIterator#
typedef struct otMeshDiagIp6AddrIterator otMeshDiagIp6AddrIterator
An opaque iterator to iterate over list of IPv6 addresses of a router.
Pointers to instance of this type are provided in otMeshDiagRouterInfo. 
otMeshDiagChildIterator#
typedef struct otMeshDiagChildIterator otMeshDiagChildIterator
An opaque iterator to iterate over list of children of a router.
Pointers to instance of this type are provided in otMeshDiagRouterInfo. 
otMeshDiagRouterInfo#
typedef struct otMeshDiagRouterInfo otMeshDiagRouterInfo
Represents information about a router in Thread mesh discovered using otMeshDiagDiscoverTopology(). 
otMeshDiagChildInfo#
typedef struct otMeshDiagChildInfo otMeshDiagChildInfo
Represents information about a discovered child in Thread mesh using otMeshDiagDiscoverTopology(). 
otMeshDiagDiscoverCallback#
typedef void(* otMeshDiagDiscoverCallback) (otError aError, otMeshDiagRouterInfo *aRouterInfo, void *aContext) )(otError aError, otMeshDiagRouterInfo *aRouterInfo, void *aContext)
Pointer type represents the callback used by otMeshDiagDiscoverTopology() to provide information about a discovered router. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aError | OT_ERROR_PENDING Indicates there are more routers to be discovered. OT_ERROR_NONE Indicates this is the last router and mesh discovery is done. OT_ERROR_RESPONSE_TIMEOUT Timed out waiting for response from one or more routers. | |
| [in] | aRouterInfo | The discovered router info (can be null if  | |
| [in] | aContext | Application-specific context. | 
When aError is OT_ERROR_PENDING, it indicates that the discovery is not yet finished and there will be more routers to discover and the callback will be invoked again.
otMeshDiagChildEntry#
typedef struct otMeshDiagChildEntry otMeshDiagChildEntry
Represents information about a child entry from otMeshDiagQueryChildTable(). 
mSupportsErrRate indicates whether or not the error tracking feature is supported and mFrameErrorRate and mMessageErrorRate values are valid. The frame error rate tracks frame tx errors (towards the child) at MAC layer, while mMessageErrorRate tracks the IPv6 message error rate (above MAC layer and after MAC retries) when an IPv6 message is dropped. For example, if the message is large and requires 6LoWPAN fragmentation, message tx is considered as failed if one of its fragment frame tx fails (for example, never acked). 
otMeshDiagQueryChildTableCallback#
typedef void(* otMeshDiagQueryChildTableCallback) (otError aError, const otMeshDiagChildEntry *aChildEntry, void *aContext) )(otError aError, const otMeshDiagChildEntry *aChildEntry, void *aContext)
Represents the callback used by otMeshDiagQueryChildTable() to provide information about child table entries. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aError | OT_ERROR_PENDING Indicates there are more entries in the table. OT_ERROR_NONE Indicates the table is finished. OT_ERROR_RESPONSE_TIMEOUT Timed out waiting for response. | |
| [in] | aChildEntry | The child entry (can be null if  | |
| [in] | aContext | Application-specific context. | 
When aError is OT_ERROR_PENDING, it indicates that the table still has more entries and the callback will be invoked again.
otMeshDiagChildIp6AddrsCallback#
typedef void(* otMeshDiagChildIp6AddrsCallback) (otError aError, uint16_t aChildRloc16, otMeshDiagIp6AddrIterator *aIp6AddrIterator, void *aContext) )(otError aError, uint16_t aChildRloc16, otMeshDiagIp6AddrIterator *aIp6AddrIterator, void *aContext)
Represents the callback used by otMeshDiagQueryChildrenIp6Addrs() to provide information about an MTD child and its list of IPv6 addresses. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aError | OT_ERROR_PENDING Indicates there are more children in the table. OT_ERROR_NONE Indicates the table is finished. OT_ERROR_RESPONSE_TIMEOUT Timed out waiting for response. | |
| [in] | aChildRloc16 | The RLOC16 of the child.  | |
| [in] | aIp6AddrIterator | An iterator to go through the IPv6 addresses of the child with  | |
| [in] | aContext | Application-specific context. | 
When aError is OT_ERROR_PENDING, it indicates that there are more children and the callback will be invoked again.
otMeshDiagRouterNeighborEntry#
typedef struct otMeshDiagRouterNeighborEntry otMeshDiagRouterNeighborEntry
Represents information about a router neighbor entry from otMeshDiagQueryRouterNeighborTable(). 
mSupportsErrRate indicates whether or not the error tracking feature is supported and mFrameErrorRate and mMessageErrorRate values are valid. The frame error rate tracks frame tx errors (towards the child) at MAC layer, while mMessageErrorRate tracks the IPv6 message error rate (above MAC layer and after MAC retries) when an IPv6 message is dropped. For example, if the message is large and requires 6LoWPAN fragmentation, message tx is considered as failed if one of its fragment frame tx fails (for example, never acked). 
otMeshDiagQueryRouterNeighborTableCallback#
typedef void(* otMeshDiagQueryRouterNeighborTableCallback) (otError aError, const otMeshDiagRouterNeighborEntry *aNeighborEntry, void *aContext) )(otError aError, const otMeshDiagRouterNeighborEntry *aNeighborEntry, void *aContext)
Represents the callback used by otMeshDiagQueryRouterNeighborTable() to provide information about neighbor router table entries. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aError | OT_ERROR_PENDING Indicates there are more entries in the table. OT_ERROR_NONE Indicates the table is finished. OT_ERROR_RESPONSE_TIMEOUT Timed out waiting for response. | |
| [in] | aNeighborEntry | The neighbor entry (can be null if  | |
| [in] | aContext | Application-specific context. | 
When aError is OT_ERROR_PENDING, it indicates that the table still has more entries and the callback will be invoked again.
Function Documentation#
otMeshDiagDiscoverTopology#
otError otMeshDiagDiscoverTopology (otInstance * aInstance, const otMeshDiagDiscoverConfig * aConfig, otMeshDiagDiscoverCallback aCallback, void * aContext)
Starts network topology discovery.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| const otMeshDiagDiscoverConfig * | [in] | aConfig | The configuration to use for discovery (e.g., which items to discover). | 
| otMeshDiagDiscoverCallback | [in] | aCallback | The callback to report the discovered routers. | 
| void * | [in] | aContext | A context to pass in  | 
otMeshDiagCancel#
void otMeshDiagCancel (otInstance * aInstance)
Cancels an ongoing topology discovery if there is one, otherwise no action.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | N/A | aInstance | 
When ongoing discovery is cancelled, the callback from otMeshDiagDiscoverTopology() will not be called anymore. 
otMeshDiagGetNextIp6Address#
otError otMeshDiagGetNextIp6Address (otMeshDiagIp6AddrIterator * aIterator, otIp6Address * aIp6Address)
Iterates through the discovered IPv6 addresses of a router or an MTD child.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otMeshDiagIp6AddrIterator * | [inout] | aIterator | The address iterator to use. | 
| otIp6Address * | [out] | aIp6Address | A pointer to return the next IPv6 address (if any). | 
MUST be used
- from the callback - otMeshDiagDiscoverCallback()and use the- mIp6AddrIteratorfrom the- aRouterInfostruct that is provided as input to the callback, or
- from the callback - otMeshDiagChildIp6AddrsCallback()along with provided- aIp6AddrIterator.
otMeshDiagGetNextChildInfo#
otError otMeshDiagGetNextChildInfo (otMeshDiagChildIterator * aIterator, otMeshDiagChildInfo * aChildInfo)
Iterates through the discovered children of a router.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otMeshDiagChildIterator * | [inout] | aIterator | The address iterator to use. | 
| otMeshDiagChildInfo * | [out] | aChildInfo | A pointer to return the child info (if any). | 
This function MUST be used from the callback otMeshDiagDiscoverCallback() and use the mChildIterator from the aRouterInfo struct that is provided as input to the callback.
otMeshDiagQueryChildTable#
otError otMeshDiagQueryChildTable (otInstance * aInstance, uint16_t aRloc16, otMeshDiagQueryChildTableCallback aCallback, void * aContext)
Starts query for child table for a given router.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| uint16_t | [in] | aRloc16 | The RLOC16 of router to query. | 
| otMeshDiagQueryChildTableCallback | [in] | aCallback | The callback to report the queried child table. | 
| void * | [in] | aContext | A context to pass in  | 
otMeshDiagQueryChildrenIp6Addrs#
otError otMeshDiagQueryChildrenIp6Addrs (otInstance * aInstance, uint16_t aRloc16, otMeshDiagChildIp6AddrsCallback aCallback, void * aContext)
Sends a query to a parent to retrieve the IPv6 addresses of all its MTD children.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| uint16_t | [in] | aRloc16 | The RLOC16 of parent to query. | 
| otMeshDiagChildIp6AddrsCallback | [in] | aCallback | The callback to report the queried child IPv6 address list. | 
| void * | [in] | aContext | A context to pass in  | 
otMeshDiagQueryRouterNeighborTable#
otError otMeshDiagQueryRouterNeighborTable (otInstance * aInstance, uint16_t aRloc16, otMeshDiagQueryRouterNeighborTableCallback aCallback, void * aContext)
Starts query for router neighbor table for a given router.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| uint16_t | [in] | aRloc16 | The RLOC16 of router to query. | 
| otMeshDiagQueryRouterNeighborTableCallback | [in] | aCallback | The callback to report the queried table. | 
| void * | [in] | aContext | A context to pass in  |