Infrastructure Interface#
This module includes the platform abstraction for the adjacent infrastructure network interface.
Functions#
Tells whether an infra interface has the given IPv6 address assigned.
Sends an ICMPv6 Neighbor Discovery message on given infrastructure interface.
The infra interface driver calls this method to notify OpenThread that an ICMPv6 Neighbor Discovery message is received.
The infra interface driver calls this method to notify OpenThread of the interface state changes.
Send a request to discover the NAT64 prefix on the infrastructure interface with aInfraIfIndex.
The infra interface driver calls this method to notify OpenThread that the discovery of NAT64 prefix is done.
Get the link-layer address of the infrastructure interface.
Enables or disables listening for DHCPv6 Prefix Delegation (PD) messages on client.
Sends a DHCPv6 message to a unicast or multicast destination address.
Callback from the platform to notify the OpenThread stack of a received DHCPv6 message.
Function Documentation#
otPlatInfraIfHasAddress#
bool otPlatInfraIfHasAddress (uint32_t aInfraIfIndex, const otIp6Address * aAddress)
Tells whether an infra interface has the given IPv6 address assigned.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aInfraIfIndex | The index of the infra interface. |
| const otIp6Address * | [in] | aAddress | The IPv6 address. |
Returns
TRUE if the infra interface has given IPv6 address assigned, FALSE otherwise.
otPlatInfraIfSendIcmp6Nd#
otError otPlatInfraIfSendIcmp6Nd (uint32_t aInfraIfIndex, const otIp6Address * aDestAddress, const uint8_t * aBuffer, uint16_t aBufferLength)
Sends an ICMPv6 Neighbor Discovery message on given infrastructure interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface this message is sent to. |
| const otIp6Address * | [in] | aDestAddress | The destination address this message is sent to. |
| const uint8_t * | [in] | aBuffer | The ICMPv6 message buffer. The ICMPv6 checksum is left zero and the platform should do the checksum calculate. |
| uint16_t | [in] | aBufferLength | The length of the message buffer. |
See RFC 4861: https://tools.ietf.org/html/rfc4861.
Note
Per RFC 4861, the implementation should send the message with IPv6 link-local source address of interface
aInfraIfIndexand IP Hop Limit 255.
otPlatInfraIfRecvIcmp6Nd#
void otPlatInfraIfRecvIcmp6Nd (otInstance * aInstance, uint32_t aInfraIfIndex, const otIp6Address * aSrcAddress, const uint8_t * aBuffer, uint16_t aBufferLength)
The infra interface driver calls this method to notify OpenThread that an ICMPv6 Neighbor Discovery message is received.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface on which the ICMPv6 message is received. |
| const otIp6Address * | [in] | aSrcAddress | The source address this message is received from. |
| const uint8_t * | [in] | aBuffer | The ICMPv6 message buffer. |
| uint16_t | [in] | aBufferLength | The length of the ICMPv6 message buffer. |
See RFC 4861: https://tools.ietf.org/html/rfc4861.
Note
Per RFC 4861, the caller should enforce that the source address MUST be a IPv6 link-local address and the IP Hop Limit MUST be 255.
otPlatInfraIfStateChanged#
otError otPlatInfraIfStateChanged (otInstance * aInstance, uint32_t aInfraIfIndex, bool aIsRunning)
The infra interface driver calls this method to notify OpenThread of the interface state changes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface. |
| bool | [in] | aIsRunning | A boolean that indicates whether the infrastructure interface is running. |
It is fine for the platform to call to method even when the running state of the interface hasn't changed. In this case, the Routing Manager state is not affected.
otPlatInfraIfDiscoverNat64Prefix#
otError otPlatInfraIfDiscoverNat64Prefix (uint32_t aInfraIfIndex)
Send a request to discover the NAT64 prefix on the infrastructure interface with aInfraIfIndex.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface to discover the NAT64 prefix. |
OpenThread will call this method periodically to monitor the presence or change of NAT64 prefix.
otPlatInfraIfDiscoverNat64PrefixDone#
void otPlatInfraIfDiscoverNat64PrefixDone (otInstance * aInstance, uint32_t aInfraIfIndex, const otIp6Prefix * aIp6Prefix)
The infra interface driver calls this method to notify OpenThread that the discovery of NAT64 prefix is done.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface on which the NAT64 prefix is discovered. |
| const otIp6Prefix * | [in] | aIp6Prefix | A pointer to NAT64 prefix. |
Is expected to be invoked after calling otPlatInfraIfDiscoverNat64Prefix. If no NAT64 prefix is discovered, aIp6Prefix shall point to an empty prefix with zero length.
otPlatGetInfraIfLinkLayerAddress#
otError otPlatGetInfraIfLinkLayerAddress (otInstance * aInstance, uint32_t aIfIndex, otPlatInfraIfLinkLayerAddress * aInfraIfLinkLayerAddress)
Get the link-layer address of the infrastructure interface.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint32_t | [in] | aIfIndex | The index of the infrastructure interface. |
| otPlatInfraIfLinkLayerAddress * | [out] | aInfraIfLinkLayerAddress | A pointer to infrastructure interface link-layer address. |
OpenThread invokes this method when the address is required, for example: when generating an ND6 message which includes a source link-layer address option.
otPlatInfraIfDhcp6PdClientSetListeningEnabled#
void otPlatInfraIfDhcp6PdClientSetListeningEnabled (otInstance * aInstance, bool aEnable, uint32_t aInfraIfIndex)
Enables or disables listening for DHCPv6 Prefix Delegation (PD) messages on client.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. |
| bool | [in] | aEnable | A boolean to enable ( |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface to operate on. |
This function is only used when OPENTHREAD_CONFIG_BORDER_ROUTING_DHCP6_PD_CLIENT_ENABLE is enabled.
When enabled, the platform must open a UDP socket on the specified infrastructure interface, binding to the DHCPv6 client port 546 to receive messages from DHCPv6 servers.
otPlatInfraIfDhcp6PdClientSend#
void otPlatInfraIfDhcp6PdClientSend (otInstance * aInstance, otMessage * aMessage, otIp6Address * aDestAddress, uint32_t aInfraIfIndex)
Sends a DHCPv6 message to a unicast or multicast destination address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. |
| otMessage * | [in] | aMessage | An |
| otIp6Address * | [in] | aDestAddress | The IPv6 multicast or unicast destination address. |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface from which to send the message. |
This function is only used when OPENTHREAD_CONFIG_BORDER_ROUTING_DHCP6_PD_CLIENT_ENABLE is enabled.
The platform is responsible for constructing a UDP datagram with the given DHCPv6 message as its payload. The datagram must be sent from the DHCPv6 client port (546) to the server port (547) on the specified infrastructure interface. The destination IPv6 address can be a unicast address or the multicast All_DHCP_Relay_Agents_and_Servers address (ff02::1:2).
This function passes the ownership of aMessage to the platform layer. Platform MUST then free the message when no longer needed.
otPlatInfraIfDhcp6PdClientHandleReceived#
void otPlatInfraIfDhcp6PdClientHandleReceived (otInstance * aInstance, otMessage * aMessage, uint32_t aInfraIfIndex)
Callback from the platform to notify the OpenThread stack of a received DHCPv6 message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. |
| otMessage * | [in] | aMessage | The |
| uint32_t | [in] | aInfraIfIndex | The index of the infrastructure interface from which the message was received.. |
This function is provided when OPENTHREAD_CONFIG_BORDER_ROUTING_DHCP6_PD_CLIENT_ENABLE is enabled.
The platform calls this function whenever a DHCPv6 message is received on the client port (546) while listening on this port is enabled (refer to otPlatInfraIfDhcp6PdClientSetListeningEnabled()).
The platform is responsible for allocating the otMessage to pass the received UDP payload. Ownership of the aMessage is passed to the OpenThread stack (which will free it once no longer needed).