A configuration for antenna selection.

Public Attributes#

bool

Antenna 0 Pin Enable.

bool

Antenna 1 Pin Enable.

uint8_t

Antenna 0 location for pin/port (EFR32 series 1) On EFR32 series 2 this field is called defaultPath and specifies the internal default RF path.

uint8_t

Antenna 0 output GPIO port.

uint8_t

Antenna 0 output GPIO pin.

uint8_t

Antenna 1 location for pin/port (EFR32 series 1 only)

uint8_t

Antenna 1 output GPIO port.

uint8_t

Antenna 1 output GPIO pin.

Public Attribute Documentation#

ant0PinEn#

bool RAIL_AntennaConfig_t::ant0PinEn

Antenna 0 Pin Enable.


ant1PinEn#

bool RAIL_AntennaConfig_t::ant1PinEn

Antenna 1 Pin Enable.


ant0Loc#

uint8_t RAIL_AntennaConfig_t::ant0Loc

Antenna 0 location for pin/port (EFR32 series 1) On EFR32 series 2 this field is called defaultPath and specifies the internal default RF path.

It is ignored on EFR32 series 2 parts that have only one RF path bonded out and on EFR32xG27 dual-band OPNs where the appropriate RF path is automatically set by RAIL to 0 for 2.4GHZ band and 1 for SubGHz band PHYs.


ant0Port#

uint8_t RAIL_AntennaConfig_t::ant0Port

Antenna 0 output GPIO port.


ant0Pin#

uint8_t RAIL_AntennaConfig_t::ant0Pin

Antenna 0 output GPIO pin.


ant1Loc#

uint8_t RAIL_AntennaConfig_t::ant1Loc

Antenna 1 location for pin/port (EFR32 series 1 only)


ant1Port#

uint8_t RAIL_AntennaConfig_t::ant1Port

Antenna 1 output GPIO port.


ant1Pin#

uint8_t RAIL_AntennaConfig_t::ant1Pin

Antenna 1 output GPIO pin.