Detailed information requested about the packet that was just, or is currently being, transmitted.
Public Attributes#
The timestamp of the transmitted packet in the RAIL timebase, filled in by RAIL_GetTxPacketDetails().
bool
Indicate whether the transmitted packet was an automatic ACK.
Public Attribute Documentation#
timeSent#
RAIL_PacketTimeStamp_t RAIL_TxPacketDetails_t::timeSent
The timestamp of the transmitted packet in the RAIL timebase, filled in by RAIL_GetTxPacketDetails().
Definition at line
3122
of file common/rail_types.h
isAck#
bool RAIL_TxPacketDetails_t::isAck
Indicate whether the transmitted packet was an automatic ACK.
In a generic sense, an automatic ACK is defined as a packet sent in response to a received ACK-requesting frame when auto-ACK is enabled. In a protocol specific sense this definition may be more or less restrictive to match the specification and you should refer to that protocol's documentation.
Definition at line
3130
of file common/rail_types.h