Built-in PHYs for alternate HFXO frequencies#
RAIL Utility for built-in PHYs#
This optional software component can be enabled to override the built-in PHYs used to support standards-based protocols based on the HFXO frequency configured as part of the device_init_hfxo component.
Currently the following combinations of chips and frequencies are supported:
EFR32XG24: 38.4 MHz, 39 MHz and 40 MHz
On unsupported chips, this component is safe to include, and will have no effect.