RF Path Utility#
RAIL RF Path Utility#
This optional software component can be enabled to include default functionality related to device-internal and device-external RF path configuration.
When using a Silicon Labs-developed board, the configuration options for this software component are set up automatically based on the selected board. When using a custom board, manually configure the configuration options.
Configuration Options#
The following configuration options can be changed:
Device-internal (EFR32XG21 only)
Switch between 2 RF paths (i.e., device pins).